Post Go back to editing

Are ADIN1200 and ADIN1300 supported by U-Boot?

Thread Summary

The user inquires about using the ADIN1300 and ADIN1200 with U-boot for cleaner initialization on a Beagleboard variant. The final answer confirms that these devices, with IEEE 802.3 compliant MII, RMII, and RGMII interfaces, should work with the generic PHY driver in U-boot. The accompanying answer asks if the ADIN1300/ADIN1200 Linux driver is supported by U-boot for booting Linux over Ethernet, suggesting it might be a No-OS driver.
AI Generated Content

I've seen the application notes on manual configuration.  Specifically I have a Beagleboard variant that I'm using an ADIN1300 and ADIN1200 on.  A U-boot initialization will be a lot cleaner.