ADIN1300: FAQ

  • Created
Was this helpful?
  • ADIN1300 Exposed paddle and Keepout area

    Original Question: ADIN1300 Exposed paddle and Keepout area by CatherineR There is an exposed paddle under the ADIN1300 package, and two keepout areas adjacent to the paddle on the package, what are…
  • ADIN1300 Gigabit Ethernet PHY Bootstrapping

    Original Question: FAQ: ADIN1300 Gigabit Ethernet PHY Bootstrapping by CatherineR Q: What PHY features can be bootstrapped at power up? A: The PHYs hardware configuration pins allow users to predefine…
  • ADIN1300 Typical Link Times FAQ

    What are the typical link times for the various modes? For the ADIN1300 Gigabit PHY Speed Configurations, where the local & remote nodes are configured the same, a link will be established in typically…
  • Are ADIN1200 and ADIN1300 supported by U-Boot?

    Original Question: Are ADIN1200 and ADIN1300 supported by U-Boot? by JDuquette210 I've seen the application notes on manual configuration. Specifically I have a Beagleboard variant that I'm using an…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.