Post Go back to editing
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Regarding the host mode configuration

Thread Summary

The user inquires about the limitations and trade-offs of configuring ADIN3310/ADIN6310 switches using SPI Host Mode and Ethernet Host Mode. In SPI Host Mode, all ports face the network, but throughput is impacted by the internal packet assist engine, and TIMER0 is unavailable for TSN functions. In Ethernet Host Mode, the host port supports high-throughput, low-latency, and deterministic TSN traffic, but the switch does not configure the PHY on the host port. The host interface is latched at reset and cannot be changed at runtime.
AI Generated Content
Category: Software
Product Number: ADIN6310
Software Version: NA

The ADIN3310/ADIN6310 switches can be configured using either SPI Host Mode or Ethernet Host Mode. Could you please clarify the limitations and trade-offs of using Ethernet Host Mode for switch configuration and management? Similarly, what are the limitations, constraints, or feature restrictions when using SPI Host Mode for switch configuration ?

Edit Notes


[locked by: CatherineR at 7:53 PM (GMT -4) on 29 Oct 2026]

Thread Notes

  • Hello,

    Thanks for your message.

    Both host modes use the same driver API and expose the same switch features, the choice depends on how much traffic your host handles and how many ports you need facing the network.

    Use SPI host mode if the host only configures and monitors the switch, with low-rate or non-time-critical traffic. All ports face the network (6 on ADIN6310, 3 on ADIN3310), no host-side PHY is needed, and it's the default if no strapping resistors are fitted. Trade-offs: any data plane traffic to/from SPI has to go to the internal packet assist engine, there's an overhead there that impacts throughput, Additionally, TIMER0 is used as the host interrupt so it's unavailable for timer/TSN functions. 

    Use Ethernet host mode if the host is itself an active talker/listener needing high throughput, low latency or deterministic TSN traffic. The host port carries both control plane and data plane, so you aren't sacrificing a port for management, you simply have 5 (ADIN6310) or 2 (ADIN3310) ports facing the external network. In a typical application this is a direct MAC-to-MAC connection with no PHY in the path, so the switch performs no PHY configuration on that port; just ensure the interface type, speed and any RGMII clock delays match on both sides via the strapping. If your design does place a PHY on the host port, the switch will not configure it: it must be strapped unmanaged, link up on its own at the speed set by the switch strapping, and present an active-low link status.

    If you need both, strap for one interface and enable the second in software during initial config e.g. SPI for control, Ethernet for data.

    Please decide at schematic stage: the host interface is latched from strapping pins at reset and cannot be changed at run time.

    Hope that helps,

    best regards,

    Catherine

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.