P4 & P5 are two ADIN110 media converter ports of our T1L 3 port switch.
They are typically used to pass T1L signal for concatenated links; downstream link connects to P4 upstream link connects to P5. P3 is a node port on the switch and not of interest here.
Object: In the event of power fail (VDD=0V) to the switch, we want to bypass the switch and connect P5 directly to P4. Basically, splicing P5 to P4 using a DPST relay for the wire pair.
We’ve implemented and preliminarily tested this using a DPDT relay.
Question:
Since P4 circuitry is still connected during power off for the splice to be enabled, the concern is that this may introduce a mismatching impedance to the spliced 110 ohm 2 wire cable.
- We would like to know when ADIN1100 is powered off, is there a low impedance pathway between TXN & TXP pins, as the concern is that it would introduce 49.9+49.9 to the differential pair?
- Or are there potentially other concerns, other than the obvious that could be introduced by the external DPDT relay?
- Or turn on substrate diodes… limited by 49.9 ohm are activated
- or...
Thanks..jonathan