Post Go back to editing

No voltage on the DLDO1_1P1

Thread Summary

The user encountered an issue where the DLDO1_1P1 output was 0V on the ADIN2111, despite no shorts to ground. The problem was resolved by correctly connecting the AVDD_L pin (Pin 36) in the schematic. The datasheet should have clarified that AVDD_L supplies the DLDO1_1P1 internal regulator.
AI Generated Content
Category: Hardware
Product Number: ADIN2111

Hello there,

has anyone encountered this problem? The same rail, 3.3V, is used to supply the ADIN2111 AVDD_H, AVDD_L, and VDDIO supply rails. Both DVDDx_1P1 1.1 V rails are being supplied from their internally DLDOx_1P1 1.1 V power supplies. There is an output voltage of 1.1 V on the DLDO2_1P1, but the DLDO1_1P1 output is 0 V. There are no shorts between DLDO1_1P1 and DVDD1_1P1 pins to the ground or any other pins or traces.  Do you know what the problem might be? Your help is greatly appreciated.   

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.