Post Go back to editing

TSN IEEE 802.1AS , ADIN6310 gPTP Slave Fails to Detect/Sync to AM62 Master (BMCA Conflict)

Thread Summary

The user is experiencing PTP synchronization failure between ADIN6310 and AM62 in Peer-to-Peer mode. The issue was resolved by configuring a valid IP address for the eth0 interface on the AM62 and correcting the destination MAC address format in ptp.cfg to use colons (01:80:C2:00:00:0E). The ADIN6310 now correctly transitions to the SLAVE state and synchronizes with the AM62 Grandmaster.
AI Generated Content
Category: Software
Product Number: ADIN6310
Software Version: version 5.1.0

ADIN6310(Master) with -AM62 (as slave) (Peer-to-Peer Mode)

ADIN 6310 as Master configuration

ref :image 1



Am62 configuration as Slave 

command: ptp4l -i eth0 -H -2 -m -q -l 6 -f gptp_custom.cfg

gptp_custom.cfg
[global]
transportSpecific        1
domainNumber           0
clientOnly                   1
logSyncInterval          -3
logAnnounceInterval    0
priority1                        255
delay_mechanism        P2P

output status 
 Adin 6310 ref iamge 2.


 AM62 output:
    ptp4l[4534.688]: selected /dev/ptp0 as PTP clock
    ptp4l[4534.742]: port 1 (eth0): INITIALIZING to LISTENING on INIT_COMPLETE
    ptp4l[4534.742]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLET
    ptp4l[4538.549]: port 1 (eth0): LISTENING to UNCALIBRATED on RS_SLAVE
    ptp4l[4539.024]: port 1 (eth0): UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED
    ptp4l[4539.650]: rms 163212 max 324892 freq -38074 +/- 14495 delay   240 +/-   0
    ptp4l[4540.650]: rms 3896 max 5970 freq -25301 +/- 5287 delay   241 +/-   0
    ptp4l[4541.650]: rms 6489 max 6804 freq -13500 +/- 1711 delay   240 +/-   0
    ptp4l[4542.649]: rms 4105 max 5459 freq -11222 +/- 166 delay   241 +/-   0
    ptp4l[4543.649]: rms 1326 max 2193 freq -12485 +/- 481 delay   240 +/-   0
    ptp4l[4544.649]: rms  237 max  369 freq -13884 +/- 302 delay   240 +/-   0
    ptp4l[4545.649]: rms  390 max  406 freq -14558 +/- 104 delay   240 +/-   0
    ptp4l[4546.649]: rms  257 max  333 freq -14715 +/-  11 delay   240 +/-   0
    ptp4l[4547.649]: rms   86 max  144 freq -14640 +/-  34 delay   240 +/-   0
    ptp4l[4548.649]: rms   24 max   33 freq -14529 +/-  23 delay   239 +/-   0
    ptp4l[4549.649]: rms   28 max   33 freq -14490 +/-   6 delay   241 +/-   0
    ptp4l[4550.649]: rms   12 max   18 freq -14493 +/-   5 delay   241 +/-   0
    ptp4l[4551.649]: rms    6 max   11 freq -14495 +/-   5 delay   241 +/-   0
    ptp4l[4552.649]: rms    6 max   11 freq -14490 +/-   5 delay   241 +/-   0
    ptp4l[4553.649]: rms    9 max   12 freq -14478 +/-   6 delay   241 +/-   0
    ptp4l[4554.649]: rms    5 max    7 freq -14487 +/-   7 delay   242 +/-   0
    ptp4l[4555.649]: rms    7 max   15 freq -14488 +/-   9 delay   242 +/-   0

pcap LOG :
    84 7.849925 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    85 7.850069 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    86 7.974904 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    87 7.975067 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    88 7.999743 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Announce Message
    89 7.999857 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 78 Signalling Message
    90 8.000015 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    91 8.000133 08:04:b4:31:12:42 LLDP_Multicast PTPv2 68 Peer_Delay_Resp Message
    92 8.000206 08:04:b4:31:12:42 LLDP_Multicast PTPv2 68 Peer_Delay_Resp_Follow_Up Message
    93 8.099926 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    94 8.100109 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    95 8.224866 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    96 8.225059 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    97 8.331701 08:04:b4:31:12:42 LLDP_Multicast PTPv2 68 Peer_Delay_Req Message
    98 8.331933 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Resp Message
    

ADIN6310 with -AM62 (Peer-to-Peer Mode)

Component                 Role    MAC Address            Sync Interval
Grandmaster (GM)    AM62 Host    c0:d6:0a:f9:69:c9    1/8 s (125 ms)
Network Device    ADIN6310 Switch    7a:c6:bb:11:11:13    Intended Slave/Boundary Clock

The ADIN6310 is configured in P2P (Peer-to-Peer) mode and intended to be a Slave to the AM62 Master. 
Synchronization is failing because the ADIN is running as a competing Master or Grandmaster (GM).

The packet trace shows the ADIN (7a:c6:bb:11:11:13) is actively transmitting its own Sync and Follow_Up messages, 
which should only be done by the elected GM. The AM62's Announce messages are being ignored, and the ADIN is not transitioning to the Slave state.

ADIN 6310 as Slave configuration

ref :image 3



Am62 configuration as Slave 

command: ptp4l -2 -H -i eth0 -m -l 6 -f gptp_custom_master.cfg

gptp_custom_master.cfg

[global]
transportSpecific       1
domainNumber            0
priority1               10
logSyncInterval         -3
logAnnounceInterval     0
delay_mechanism         P2P

output status 
 
 AM62 output:
    ptp4l[1356.082]: selected /dev/ptp0 as PTP clock
    ptp4l[1356.116]: port 1 (eth0): INITIALIZING to LISTENING on INIT_COMPLETE
    ptp4l[1356.116]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
    ptp4l[1356.116]: port 0 (/var/run/ptp4lro): INITIALIZING to LISTENING on INIT_COMPLETE
    ptp4l[1357.919]: port 1 (eth0): new foreign master 7ac6bb.1111.110000-1
    ptp4l[1359.529]: port 1 (eth0): LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
    ptp4l[1359.529]: selected local clock 0804b4.fffe.3112ea as best master
    ptp4l[1359.529]: port 1 (eth0): assuming the grand master role
 
 Adin 6310 ref iamge 4.


 
PCAP LOG

     30.688251 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     30.688370 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     30.813268 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     30.813323 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     30.938289 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     30.938340 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     30.961916 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 78 Signalling Message
     30.962056 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
     30.962141 c0:d6:0a:f9:69:c9 LLDP_Multicast PTPv2 68 Peer_Delay_Resp Message
     30.962184 c0:d6:0a:f9:69:c9 LLDP_Multicast PTPv2 68 Peer_Delay_Resp_Follow_Up Message
     30.962578 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Announce Message
     31.000973 c0:d6:0a:f9:69:c9 LLDP_Multicast PTPv2 68 Peer_Delay_Req Message
     31.001231 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Resp Message
     31.001330 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Resp_Follow_Up Message
     31.056993 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     31.057204 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     31.063326 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     31.063371 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     31.182004 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     31.182200 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     31.188345 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     31.188398 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     31.307013 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     31.307199 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     31.307376 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 78 Announce Message
     31.313373 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     31.313428 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     31.432004 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     31.432197 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     31.438402 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     31.438457 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     31.556998 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     31.557195 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     31.563437 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     31.563500 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     31.682008 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     31.682194 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     31.688472 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     31.688519 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     31.806995 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     31.807192 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     31.813493 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     31.813547 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     31.931989 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     31.932189 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     31.938513 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     31.938562 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     31.961865 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Announce Message
     31.961981 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 78 Signalling Message
     31.962140 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
     31.962180 c0:d6:0a:f9:69:c9 LLDP_Multicast PTPv2 68 Peer_Delay_Resp Message
     31.962216 c0:d6:0a:f9:69:c9 LLDP_Multicast PTPv2 68 Peer_Delay_Resp_Follow_Up Message
     32.000978 c0:d6:0a:f9:69:c9 LLDP_Multicast PTPv2 68 Peer_Delay_Req Message
     32.001196 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Resp Message
     32.001312 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Resp_Follow_Up Message
     32.056986 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     32.057186 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     32.063543 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     32.063592 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     32.181985 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     32.182185 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     32.188566 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     32.188615 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message
     32.306990 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
     32.307183 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
     32.307395 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 78 Announce Message
     32.313594 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Sync Message
     32.313644 c0:d6:0a:f9:69:c9 IeeeI&MS_00:00:00 PTPv2 58 Follow_Up Message

Thread Notes

Parents
  • Hi Dhevak,

    Are you currently using software version v5.1.0?

    We tested the same scenario using v5.1.0, where a Linux PC was configured as the GM and connected to ADIN6310 physical port 2 (PTP port 3). It appears to be working well, the ADIN6310 is successfully synchronizing with the Grandmaster (Linux PC). Could you please share a Wireshark capture from your setup?

    I’m also attaching screenshots showing the configuration, where the ADIN6310 is set to TimeReceiver mode and the Linux PC is acting as the Grandmaster for your reference.

    ADIN6310 Candidate page:

    Status page:

    GM configuration:

      

    Regards,
    Himanshu

  • Hello Himanshu,

    Thank you for confirming your successful test using v5.1.0. We are also using v5.1.0, the issue persists in our setup. The ADIN6310 is not synchronizing with our Grand master (AM62 linux processor) connected to physical port 2.

    ADIN configuration

     

    configuration status

    AM62 configuration and status

    ptp.cfg 

    [global]
    gmCapable                          1
    priority1                               10
    priority2                               255
    logAnnounceInterval           0
    logSyncInterval                  -3
    syncReceiptTimeout           3
    neighborPropDelayThresh   800
    min_neighbor_prop_delay -20000000
    assume_two_step              1
    path_trace_enabled           1
    follow_up_info                    1
    transportSpecific                 0x1
    ptp_dst_mac                       7A:C6:BB:11:11:13
    network_transport               L2
    delay_mechanism               P2P

    Command output-

    ptp4l -i eth0 -m -l 6 -f ptp.cfg 

    ptp4l[3069.217]: selected /dev/ptp0 as PTP clock
    ptp4l[3069.252]: port 1 (eth0): INITIALIZING to LISTENING on INIT_COMPLETE
    ptp4l[3069.252]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
    ptp4l[3069.253]: port 0 (/var/run/ptp4lro): INITIALIZING to LISTENING on INIT_COMPLETE
    ptp4l[3072.879]: port 1 (eth0): new foreign master 7ac6bb.1111.110000-1
    ptp4l[3073.153]: port 1 (eth0): LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
    ptp4l[3073.153]: selected local clock 0804b4.fffe.311242 as best master
    ptp4l[3073.153]: port 1 (eth0): assuming the grand master role
    ptp4l[3074.879]: selected best master clock 7ac6bb.1111.110000
    ptp4l[3074.879]: port 1 (eth0): assuming the grand master role
    ptp4l[3079.084]: port 1 (eth0): received SYNC without timestamp

    To help isolate the discrepancy between our setups, I have captured the network traffic also- using tcpdump.

    3280 101.698993 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3281 101.699192 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3282 101.788112 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3283 101.788199 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3284 101.823986 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3285 101.824191 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3286 101.913161 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3287 101.913252 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3288 101.948999 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3289 101.949191 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3290 101.993864 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Announce Message
    3291 101.993979 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 78 Signalling Message
    3292 101.994133 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    3293 101.994184 08:04:b4:31:12:42 LLDP_Multicast PTPv2 68 Peer_Delay_Resp Message
    3294 101.994230 08:04:b4:31:12:42 LLDP_Multicast PTPv2 68 Peer_Delay_Resp_Follow_Up Message
    3295 102.038166 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3296 102.038202 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3297 102.073982 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3298 102.074184 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3299 102.163195 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3300 102.163235 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3301 102.199014 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3302 102.199184 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3303 102.272906 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Announce Message
    3304 102.288226 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3305 102.288284 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3306 102.323995 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3307 102.324182 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3308 102.370812 08:04:b4:31:12:42 LLDP_Multicast PTPv2 68 Peer_Delay_Req Message
    3309 102.371030 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Resp Message
    3310 102.371152 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Resp_Follow_Up Message
    3311 102.413265 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3312 102.413326 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3313 102.448979 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3314 102.449181 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3315 102.538277 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3316 102.538319 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3317 102.573974 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3318 102.574179 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3319 102.663295 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3320 102.663333 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3321 102.698975 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3322 102.699177 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3323 102.788328 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3324 102.788387 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3325 102.823971 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3326 102.824176 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3327 102.913379 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3328 102.913462 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3329 102.948970 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3330 102.949173 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3331 102.993848 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Announce Message
    3332 102.993964 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 78 Signalling Message
    3333 102.994120 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    3334 102.994159 08:04:b4:31:12:42 LLDP_Multicast PTPv2 68 Peer_Delay_Resp Message
    3335 102.994197 08:04:b4:31:12:42 LLDP_Multicast PTPv2 68 Peer_Delay_Resp_Follow_Up Message
    3336 103.038385 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3337 103.038418 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3338 103.073972 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3339 103.074173 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3340 103.163426 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3341 103.163480 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3342 103.198966 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3343 103.199170 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3344 103.272904 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Announce Message
    3345 103.288443 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3346 103.288480 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3347 103.323970 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3348 103.324171 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3349 103.370852 08:04:b4:31:12:42 LLDP_Multicast PTPv2 68 Peer_Delay_Req Message
    3350 103.371081 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Resp Message
    3351 103.371197 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 72 Peer_Delay_Resp_Follow_Up Message
    3352 103.413480 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3353 103.413537 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3354 103.448961 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3355 103.449163 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message
    3356 103.538489 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 58 Sync Message
    3357 103.538525 08:04:b4:31:12:42 7a:c6:bb:11:11:13 PTPv2 90 Follow_Up Message
    3358 103.573956 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 64 Sync Message
    3359 103.574163 7a:c6:bb:11:11:13 LLDP_Multicast PTPv2 94 Follow_Up Message

    Here i have followed your configuration but still i am facing BMCA detectetion fails,
    were am i going wrong.
  • Hi Dhevak,

    Thank you for sharing the details.

    Upon reviewing attached ptp.cfg capture, I noticed that the "ptp_dst_mac" is currently set to the unicast MAC address "7A:C6:BB:11:11:13", which is not in line with the expected configuration. According to the AS2020 standard, the PTP destination MAC address should be set to "01-80-C2-00-00-0E". Using a unicast MAC address will result in the switch dropping the PTP packets, thereby preventing synchronization with the GM.

    I kindly request you to update the ptp_dst_mac to "01-80-C2-00-00-0E" as per the standard and try again.

    Regards,
    Himanshu 




  • Hai ,

    i have tried the configuration u mentions but still that master not detected in ADIN

    Configuration -

    [global]
    gmCapable               1
    priority1               10
    priority2               255
    logAnnounceInterval     0
    logSyncInterval         -3
    syncReceiptTimeout      3
    neighborPropDelayThresh   800
    min_neighbor_prop_delay -20000000
    assume_two_step         1
    path_trace_enabled      1
    follow_up_info          1
    transportSpecific       0x1
    ptp_dst_mac             01-80-C2-00-00-0E
    network_transport       L2
    delay_mechanism         P2P
    
     ptp4l -i eth0 -l 6 -m -q
    ptp4l[2069.626]: selected /dev/ptp0 as PTP clock
    ptp4l[2069.637]: port 1 (eth0): INITIALIZING to LISTENING on INIT_COMPLETE
    ptp4l[2069.638]: port 0 (/var/run/ptp4l): INITIALIZING to LISTENING on INIT_COMPLETE
    ptp4l[2069.638]: port 0 (/var/run/ptp4lro): INITIALIZING to LISTENING on INIT_COMPLETE
    ptp4l[2076.388]: port 1 (eth0): LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES
    ptp4l[2076.388]: selected local clock 0804b4.fffe.311242 as best master
    ptp4l[2076.388]: port 1 (eth0): assuming the grand master role

    PACP log-

    1 0.000000 0.0.0.0 224.0.1.129 PTPv2 86 Sync Message
    2 0.000179 0.0.0.0 224.0.1.129 PTPv2 86 Follow_Up Message
    3 0.156142 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 78 Signalling Message
    4 0.156267 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    5 1.000077 0.0.0.0 224.0.1.129 PTPv2 86 Sync Message
    6 1.000217 0.0.0.0 224.0.1.129 PTPv2 86 Follow_Up Message
    7 1.000272 0.0.0.0 224.0.1.129 PTPv2 106 Announce Message
    8 1.156055 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 78 Signalling Message
    9 1.156202 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    10 2.000156 0.0.0.0 224.0.1.129 PTPv2 86 Sync Message
    11 2.000277 0.0.0.0 224.0.1.129 PTPv2 86 Follow_Up Message
    12 2.156093 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 78 Signalling Message
    13 2.156234 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    14 3.000262 0.0.0.0 224.0.1.129 PTPv2 86 Sync Message
    15 3.000408 0.0.0.0 224.0.1.129 PTPv2 86 Follow_Up Message
    16 3.000468 0.0.0.0 224.0.1.129 PTPv2 106 Announce Message
    17 3.156030 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 78 Signalling Message
    18 3.156171 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    19 4.000283 0.0.0.0 224.0.1.129 PTPv2 86 Sync Message
    20 4.000380 0.0.0.0 224.0.1.129 PTPv2 86 Follow_Up Message
    21 4.156059 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 78 Signalling Message
    22 4.156200 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    23 5.000393 0.0.0.0 224.0.1.129 PTPv2 86 Sync Message
    24 5.000515 0.0.0.0 224.0.1.129 PTPv2 86 Follow_Up Message
    25 5.000569 0.0.0.0 224.0.1.129 PTPv2 106 Announce Message
    26 5.155999 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 78 Signalling Message
    27 5.156137 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    28 6.000479 0.0.0.0 224.0.1.129 PTPv2 86 Sync Message
    29 6.000614 0.0.0.0 224.0.1.129 PTPv2 86 Follow_Up Message
    30 6.156039 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 78 Signalling Message
    31 6.156168 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    32 7.000578 0.0.0.0 224.0.1.129 PTPv2 86 Sync Message
    33 7.000721 0.0.0.0 224.0.1.129 PTPv2 86 Follow_Up Message
    34 7.000778 0.0.0.0 224.0.1.129 PTPv2 106 Announce Message
    35 7.155992 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 78 Signalling Message
    36 7.156109 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message
    37 8.000677 0.0.0.0 224.0.1.129 PTPv2 86 Sync Message
    38 8.000815 0.0.0.0 224.0.1.129 PTPv2 86 Follow_Up Message
    39 8.156007 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 78 Signalling Message
    40 8.156136 7a:c6:bb:11:11:14 LLDP_Multicast PTPv2 72 Peer_Delay_Req Message

  • Hi Dhevak,

    Thank you for sharing the configuration details.

    In the PCAP log, the source address appears as 0.0.0.0. Packets with this source address will be dropped by the switch.

    Could you please verify this behavior and try again?


    Regards,
    Himanshu



    • on Nov 1, 2025 3:44 AM in reply to Hseth Contains AI Generated Content
      +1

      Hi Himanshu,

      Thank you for the crucial feedback regarding the 0.0.0.0 source address in the PCAP log. That insight was key to resolving the issue.

      I have implemented the following changes on the AM62 side:

      • IP Configuration: An IP address was successfully configured for the eth0 interface on the AM62 side. This corrected the 0.0.0.0 source address problem.

      • MAC Address Format: The destination MAC address in ptp.cfg was corrected to use colons (01:80:C2:00:00:0E) instead of hyphens (01-80-C2-00-00-0E). This ensures proper Layer 2 (Ethernet) framing, which was likely the cause of the packets being dropped or misprocessed.

       PTP Synchronization Status: Working Fine

      The result is successful PTP synchronization:

      • Status Confirmation: The ADIN6310 GUI status page now correctly confirms that the Primary Clock is found and lists the AM62 clock identity (fffe.311242). The ADIN6310 has transitioned to the SECONDARY state.

      New PCAP Trace Data (Verification)

      The new PCAP trace now shows the expected PTP multicast traffic and communication:

      PTP Message Type Source IP Destination IP Key Observation
      Announce 192.168.1.100 (AM62 Primary) 224.0.1.129 (PTP Multicast) Confirms the AM62 is correctly advertising its clock.
      Sync/Follow_Up 192.168.1.100 (AM62 Primary) 224.0.1.129 (PTP Multicast) The essential timing messages are now being sent with a valid Source IP.
      Delay_Req <ADIN6310-IP> (ADIN6310 Secondary) 192.168.1.100 (AM62 Primary) Confirms the ADIN6310 is actively communicating back to the AM62 Primary.

      The issue is resolved. Thank you again for pointing out the source address problem—that guided the correction of the network stack configuration.

      Regards, Dhevak A

    Reply
      • on Nov 1, 2025 3:44 AM in reply to Hseth Contains AI Generated Content
        +1

        Hi Himanshu,

        Thank you for the crucial feedback regarding the 0.0.0.0 source address in the PCAP log. That insight was key to resolving the issue.

        I have implemented the following changes on the AM62 side:

        • IP Configuration: An IP address was successfully configured for the eth0 interface on the AM62 side. This corrected the 0.0.0.0 source address problem.

        • MAC Address Format: The destination MAC address in ptp.cfg was corrected to use colons (01:80:C2:00:00:0E) instead of hyphens (01-80-C2-00-00-0E). This ensures proper Layer 2 (Ethernet) framing, which was likely the cause of the packets being dropped or misprocessed.

         PTP Synchronization Status: Working Fine

        The result is successful PTP synchronization:

        • Status Confirmation: The ADIN6310 GUI status page now correctly confirms that the Primary Clock is found and lists the AM62 clock identity (fffe.311242). The ADIN6310 has transitioned to the SECONDARY state.

        New PCAP Trace Data (Verification)

        The new PCAP trace now shows the expected PTP multicast traffic and communication:

        PTP Message Type Source IP Destination IP Key Observation
        Announce 192.168.1.100 (AM62 Primary) 224.0.1.129 (PTP Multicast) Confirms the AM62 is correctly advertising its clock.
        Sync/Follow_Up 192.168.1.100 (AM62 Primary) 224.0.1.129 (PTP Multicast) The essential timing messages are now being sent with a valid Source IP.
        Delay_Req <ADIN6310-IP> (ADIN6310 Secondary) 192.168.1.100 (AM62 Primary) Confirms the ADIN6310 is actively communicating back to the AM62 Primary.

        The issue is resolved. Thank you again for pointing out the source address problem—that guided the correction of the network stack configuration.

        Regards, Dhevak A

      Children
      No Data