Post Go back to editing
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Time-Sensitive Networking (TSN) Configuration and Observation Issue in IEEE 802.1Qbv (TAS)

Thread Summary

The user is troubleshooting Time-Sensitive Networking (TSN) with a Texas Instruments AM62 processor and an Analog Devices ADIN6310 switch. The issue is that traffic is not adhering to the configured GCL timings, despite VLAN 100 being configured on all boards. The final answer suggests verifying if the frames are being queued to Gate 0 and ensuring that Gate 7 is open for PTP packets. The user should also check the VLAN tags and priorities of the transmitted frames.
AI Generated Content
Category: Software
Product Number: ADIN 6310
Software Version: version 5.0

System Setup

Component               Model/Platform                               Role
Endpoint (Sender)    Texas Instruments AM62 (Linux)    Traffic Source, responsible for VLAN/PCP Tagging.
TSN Switch               Analog Devices ADIN6310            TAS Gatekeeper, responsible for Scheduling (802.1Qbv).
Synchronization        IEEE 802.1AS (gPTP)                    Configured in Boundary Mode and assumed stable.

AM62 (Sender) Configuration (Traffic Classification)

The AM62 uses Linux Traffic Control (tc) to classify UDP traffic 
DPort     tc Filter Action                    Linux skb->priority    
10001    action skbedit priority 0     0 (Highest)    
10002    action skbedit priority 1     1 (Medium)    
10003    action skbedit priority 2     2 (Lowest)    

AM62 Traffic Generation Command

The output was observed while generating high-rate traffic, likely hitting DPort 10001 with a single plget instance:

./plget -i eth0 -m pkt-gen -p 3 -t ptpl2 -n 128 -a 70:ff:76:1d:8c:08 -l 1500
sleep 5
./plget -i eth0 -m pkt-gen -p 2 -t ptpl2 -n 128 -a 70:ff:76:1d:8c:08 -l 1500
sleep 5
./plget -i eth0 -m pkt-gen -p 1 -t ptpl2 -n 128 -a 70:ff:76:1d:8c:08 -l 1500


ADIN6310 (TSN Switch) Configuration

TAS Gate Control List (GCL)

The TAS GCL was configured with three entries for three intended priority queues :
GCL Entry    Gate Duration (ns)    Gate State (Assumed Queue Index)
Entry 0         125,000                     Opens Queue for Prio 3 (e.g., Q3 - from "4th checkbox from right")
Entry 1         125,000                     Opens Queue for Prio 2 (e.g., Q1 - from "2nd checkbox from right")
Entry 2         250,000                     Opens Queue for Prio 1 (e.g., Q0 - from "1st checkbox from right")
GCL Cycle    500,000 ns (0.5 ms)    Sum of Durations

Receiver End (AM62)

command
#Bash
while sleep 1; do ./plget -m rx-lat -f ipgap -n 128 -i vlan100 -t ptpl2 -f hwts; done

Observed Output (Single Transaction Phenomenon)

The output provided below shows the inter-packet gap (IPG) from the receiver, which was identified as traffic from a single observed queue ("queue 1 with prio mof 3").

The majority of IPGs are 12.224 ms, interspersed with much larger delays, including 263.943 ms and 266.559 ms some random large gaps.

Only one transaction is appeared in output 

Clarification required : settings required for the ADIN6310 to correctly classify incoming PCP 0, 1, and 2 traffic into specific internal queues (e.g., Q3, Q1, Q0) for TAS scheduling.

Edit Notes


[locked by: CatherineR at 5:48 PM (GMT -4) on 1 Apr 2026]
Parents
  • Hi Dhevak,

    How are you trying to configure the device, through the evaluation software or the driver library? Are you using an evaluation board for testing?

    In the driver UG (UG-2287 (Rev.B)), page 80, there is an example of configuring scheduled traffic.

    You need to change the gateParam.admin_control_list[X].time_interval_value and the gateParam.admin_control_list[X].gate_state_value in the example code.

    In the eval UG (UG-2280 (Rev.B)), page 62, the default behavior of the switch is that Q0 is mapped to Priority 0, Q1 to Priority 1, Q2 to Priority 2, and so on.

    Entry 0         125,000                     Opens Queue for Prio 3 (e.g., Q3 - from "4th checkbox from right")
    Entry 1         125,000                     Opens Queue for Prio 2 (e.g., Q2 - from "3rd checkbox from right")
    Entry 2         250,000                     Opens Queue for Prio 1 (e.g., Q1 - from "2nd checkbox from right")

    Also, you need to configure the VLAN ID to learn and forward.

    Regards,

    Karl

  • Thank you for your reply.

    I am currently using the evaluation software for the ADIN6310 EVK module and have implemented the following configuration steps:

    1. VLAN Configuration: Configured VLAN 1 on the switch to be in the learning and forwarding state with default priority queue mapping.

    2. Time-Aware Shaper (TAS) Egress Configuration: Enabled the TAS schedule for egress with the following entries (Gate Control List - GCL):

      • Entry 0: 125,000 ns duration. Opens the gate for Priority Queue 3 (Prio 3)  - from "4th checkbox from right".

      • Entry 1: 125,000 ns duration. Opens the gate for Priority Queue 2 (Prio 2)  - from "3th checkbox from right".

      • Entry 2: 250,000 ns duration. Opens the gate for Priority Queue 1 (Prio 1)  - from "2th checkbox from right".

    3. End Node/Processor Configuration: The AM62 processor/node is configured with VLAN 100 and transmission was attempted through this VLAN.

    4. Traffic Generation: The traffic load was generated using the "plget" tool to measure time delay.

    5. Observation: No data was received at the end node.

    Issue: I suspect a missing or incorrect switch configuration, particularly concerning the interaction between VLAN 1 (Switch forwarding) and VLAN 100 (AM62 traffic), or how the TAS is impacting the traffic. Could you please advise if there are any critical configurations I might have missed in the switch?

  • In the VLAN table, it should look something similar to below. In the image you shared its showing VLAN ID 1.

    Can you try sending traffic without configuring the IEEE 802.1Qbv?

    This is to verify the receiver is receiving any traffic.

  • yep !  you are right 

    actually i added the wrong image

    the actual image is

     

    As for the data transmission  i have tried in Four case  here without TAS (IEEE 802.1qbv) GCL ,

    data observed in am62  Brd 2:

    case 1: AM62 - AM62 without VLAN and switch data transmission.

    output-

    cat prio
    prio1.txt  prio2.txt  prio3.txt  
    root@am62xxsip-evm:~/tsn# cat prio3.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58


    hw rx time, us: packets 128:
    relative abs time 620392458767 ns
    first packet abs time 620392458767 ns
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          12.192 |          24.384 |          52.344 |          64.536 |          76.728 |           88.92 |         101.112 |
             113.304 |         125.496 |         137.688 |          149.88 |         162.072 |         174.264 |         186.456 |         198.648 |
              210.84 |         223.032 |         235.224 |         247.416 |         259.608 |     1.84467e+16 |         283.992 |         296.184 |
             308.384 |         320.576 |         332.768 |          344.96 |         357.152 |         369.344 |         381.536 |         393.728 |
              405.92 |         418.112 |         430.304 |         442.496 |         454.688 |          466.88 |         479.072 |         491.264 |
             503.456 |         515.648 |          527.84 |         540.032 |         552.224 |         564.416 |         576.608 |           588.8 |
             600.992 |         613.184 |         625.376 |         637.568 |          649.76 |         661.952 |         674.144 |         686.336 |
             698.528 |          710.72 |         722.912 |         735.104 |         747.296 |         759.488 |          771.68 |         783.872 |
             796.064 |         808.256 |         820.448 |          832.64 |         844.832 |         857.024 |         869.216 |         881.408 |
               893.6 |         905.792 |         917.984 |         930.176 |         942.368 |          954.56 |         966.752 |         978.944 |
             991.136 |         1003.33 |         1015.52 |         1027.71 |          1039.9 |          1052.1 |         1064.29 |         1076.48 |
             1088.67 |         1100.86 |         1113.06 |         1125.25 |         1137.44 |         1149.63 |         1161.82 |         1174.02 |
             1186.21 |          1198.4 |         1210.59 |         1222.78 |         1234.98 |         1247.17 |         1259.36 |         1271.55 |
             1283.74 |         1295.94 |         1308.13 |         1320.32 |         1332.51 |          1344.7 |          1356.9 |         1369.09 |
             1381.28 |         1393.47 |         1405.66 |         1417.86 |         1430.05 |         1442.24 |         1454.43 |         1466.62 |
             1478.82 |         1491.01 |          1503.2 |         1515.39 |         1527.58 |         1539.78 |         1551.97 |         1564.16 |
    ------------------------------------------------------------------------------------------------------------------------------------------------


    gap of hw rx time, us: packets 128:
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          12.192 |          12.192 |           27.96 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |     1.84467e+16 |     6.20393e+08 |          12.192 |
                12.2 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
    ------------------------------------------------------------------------------------------------------------------------------------------------
    max val(#21) = 18446743453316832.00us
    min val(#1) = 12.19us
    peak-to-peak = 18446743453316820.00us
    mean +- RMS = 145249953336307.75 +- 1630426627218992.00 us

    frame size: 1500
    number of packets: 128
    RAW RATE = 974324.88kbps, PPS = 81193.7
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# cat prio2.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58


    hw rx time, us: packets 128:
    relative abs time 610328412503 ns
    first packet abs time 610328412503 ns
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          12.192 |          24.384 |          54.488 |           66.68 |          78.872 |          91.064 |         103.256 |
             115.448 |          127.64 |         139.832 |         152.024 |         164.216 |         176.408 |           188.6 |         200.792 |
             212.984 |         225.176 |         237.368 |          249.56 |         261.752 |         273.944 |         286.136 |         298.328 |
              310.52 |         322.712 |         334.904 |         347.096 |         359.288 |          371.48 |         383.672 |         395.864 |
             408.056 |         420.248 |          432.44 |         444.632 |         456.824 |         469.016 |         481.208 |           493.4 |
             505.592 |         517.784 |         529.976 |         542.168 |          554.36 |         566.552 |         578.744 |         590.936 |
             603.128 |          615.32 |         627.512 |         639.704 |         651.896 |         664.088 |          676.28 |         688.472 |
             700.664 |         712.856 |         725.048 |          737.24 |         749.432 |         761.624 |         773.816 |         786.008 |
               798.2 |           810.4 |         822.592 |         834.784 |         846.976 |         859.168 |          871.36 |         883.552 |
             895.744 |         907.936 |         920.128 |          932.32 |         944.512 |         956.704 |         968.896 |         981.088 |
              993.28 |         1005.47 |         1017.66 |         1029.86 |         1042.05 |         1054.24 |         1066.43 |         1078.62 |
             1090.82 |         1103.01 |          1115.2 |         1127.39 |         1139.58 |         1151.78 |         1163.97 |         1176.16 |
             1188.35 |         1200.54 |         1212.74 |         1224.93 |         1237.12 |         1249.31 |          1261.5 |          1273.7 |
             1285.89 |         1298.08 |         1310.27 |         1322.46 |         1334.66 |         1346.85 |         1359.04 |         1371.23 |
             1383.42 |         1395.62 |         1407.81 |            1420 |         1432.19 |         1444.38 |         1456.58 |         1468.77 |
             1480.96 |         1493.15 |         1505.34 |         1517.54 |         1529.73 |         1541.92 |         1554.11 |          1566.3 |
    ------------------------------------------------------------------------------------------------------------------------------------------------


    gap of hw rx time, us: packets 128:
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          12.192 |          12.192 |          30.104 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |            12.2 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
              12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |          12.192 |
    ------------------------------------------------------------------------------------------------------------------------------------------------
    max val(#3) = 30.10us
    min val(#1) = 12.19us
    peak-to-peak = 17.91us
    mean +- RMS = 12.33 +- 1.58 us

    frame size: 1500
    number of packets: 128
    RAW RATE = 972991.19kbps, PPS = 81082.6
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# cat prio1.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58

    #########################################################################

    case 2: No VLAN configuration in AM62 and Switch 

    output-

    cat prio3.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58

    frame size: 1500
    number of packets: 0
    RAW RATE = 167.70kbps, PPS = 14.0
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# cat prio2.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58

    frame size: 1500
    number of packets: 0
    RAW RATE = 168.52kbps, PPS = 14.0
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# cat prio1.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58

    frame size: 1500
    number of packets: 0
    RAW RATE = 381.82kbps, PPS = 31.8

    Observation - no of packets received is 0.

    ----------------------------------------------------------------

    case 3: VLAN 100 in switch alone 

    output-

    cat prio3.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58

    frame size: 1500
    number of packets: 0
    RAW RATE = 152.90kbps, PPS = 12.7
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# cat prio2.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58

    frame size: 1500
    number of packets: 0
    RAW RATE = 153.58kbps, PPS = 12.8
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# 
    root@am62xxsip-evm:~/tsn# cat prio1.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58

    frame size: 1500
    number of packets: 0
    RAW RATE = 1741.10kbps, PPS = 145.1

    ---------------------------------------------------------------------------------------------

    case 4: VLAN 100 in AM62 and Switch .

    command- TAS_receive.sh 
    #while sleep 1; do ./plget -m rx-lat -f ipgap -n 128 -i eth0 -t ptpl2 -f hwts; done
    ./plget -m rx-lat -f ipgap -n 128 -i eth0.100 -t ptpl2 -f hwts  > prio1.txt 
    ./plget -m rx-lat -f ipgap -n 128 -i eth0.100 -t ptpl2 -f hwts  > prio2.txt 
    ./plget -m rx-lat -f ipgap -n 128 -i eth0.100 -t ptpl2 -f hwts  > prio3.txt

    output-

     prio3.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58


    hw rx time, us: packets 128:
    relative abs time 1278681590192 ns
    first packet abs time 1278681590192 ns
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          62.992 |          76.856 |          89.504 |         102.336 |          114.88 |         126.992 |         139.144 |
             151.416 |         163.656 |         178.224 |         190.592 |         202.704 |          214.68 |         226.896 |         238.856 |
             251.384 |         263.488 |          275.68 |         287.848 |         299.832 |          311.76 |         323.888 |         335.904 |
             348.248 |           360.2 |          379.44 |         391.624 |         403.624 |         415.576 |         427.416 |         439.384 |
             451.328 |         463.192 |         474.896 |         486.896 |         498.688 |         510.584 |          522.36 |         534.208 |
             546.192 |         558.024 |         570.208 |         582.072 |         593.984 |         605.896 |          617.72 |          629.56 |
             641.688 |         653.568 |         665.312 |         677.136 |         689.128 |         701.224 |         713.344 |         725.304 |
             737.536 |         749.824 |         764.152 |         776.264 |         788.152 |         800.024 |         811.824 |          823.72 |
             835.832 |         847.704 |         859.528 |         871.384 |         883.136 |         895.016 |         906.728 |         918.528 |
             930.528 |         942.464 |         954.424 |          966.48 |           978.2 |         989.944 |         1001.54 |         1013.25 |
              1025.3 |         1037.46 |         1049.36 |         1061.26 |         1073.01 |         1084.87 |          1096.9 |         1108.74 |
             1120.78 |         1132.71 |         1146.74 |          1158.8 |         1170.78 |         1182.75 |          1194.6 |         1206.38 |
             1218.55 |         1230.39 |         1242.25 |         1254.22 |         1266.07 |         1277.76 |          1289.7 |         1301.34 |
             1313.34 |         1325.24 |         1337.19 |         1349.14 |         1360.83 |         1372.62 |          1384.5 |         1396.14 |
             1408.01 |          1419.8 |         1431.66 |         1443.26 |         1455.01 |         1466.79 |         1478.62 |         1490.58 |
             1502.55 |         1514.31 |         1528.22 |         1540.14 |         1551.97 |         1563.71 |         1575.53 |         1587.39 |
    ------------------------------------------------------------------------------------------------------------------------------------------------


    gap of hw rx time, us: packets 128:
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          62.992 |          13.864 |          12.648 |          12.832 |          12.544 |          12.112 |          12.152 |
              12.272 |           12.24 |          14.568 |          12.368 |          12.112 |          11.976 |          12.216 |           11.96 |
              12.528 |          12.104 |          12.192 |          12.168 |          11.984 |          11.928 |          12.128 |          12.016 |
              12.344 |          11.952 |           19.24 |          12.184 |              12 |          11.952 |           11.84 |          11.968 |
              11.944 |          11.864 |          11.704 |              12 |          11.792 |          11.896 |          11.776 |          11.848 |
              11.984 |          11.832 |          12.184 |          11.864 |          11.912 |          11.912 |          11.824 |           11.84 |
              12.128 |           11.88 |          11.744 |          11.824 |          11.992 |          12.096 |           12.12 |           11.96 |
              12.232 |          12.288 |          14.328 |          12.112 |          11.888 |          11.872 |            11.8 |          11.896 |
              12.112 |          11.872 |          11.824 |          11.856 |          11.752 |           11.88 |          11.712 |            11.8 |
                  12 |          11.936 |           11.96 |          12.056 |           11.72 |          11.744 |            11.6 |          11.704 |
              12.048 |           12.16 |          11.904 |          11.896 |          11.752 |          11.864 |          12.032 |           11.84 |
               12.04 |          11.928 |          14.024 |          12.064 |          11.976 |          11.976 |          11.848 |          11.784 |
              12.168 |           11.84 |          11.856 |          11.968 |          11.856 |          11.688 |          11.936 |           11.64 |
              12.008 |          11.896 |          11.952 |          11.952 |          11.688 |          11.784 |           11.88 |           11.64 |
              11.872 |          11.792 |          11.856 |          11.608 |          11.744 |          11.784 |          11.832 |          11.952 |
              11.976 |           11.76 |          13.912 |          11.912 |          11.832 |          11.744 |          11.816 |          11.864 |
    ------------------------------------------------------------------------------------------------------------------------------------------------
    max val(#1) = 62.99us
    min val(#78) = 11.60us
    peak-to-peak = 51.39us
    mean +- RMS = 12.50 +- 4.57 us

    frame size: 80
    number of packets: 128
    RAW RATE = 51203.48kbps, PPS = 80005.4

    at prio2.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58


    hw rx time, us: packets 128:
    relative abs time 1258562997688 ns
    first packet abs time 1258562997688 ns
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          46.872 |          52.568 |          59.912 |           60.92 |     1.84467e+16 |          74.304 |          75.216 |
              76.352 |          82.912 |     1.84467e+16 |          89.808 |          95.136 |          100.32 |          105.72 |         111.864 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |         271.152 |         276.336 |         281.568 |         286.864 |
             293.472 |         298.984 |         304.344 |         309.608 |         314.792 |         320.016 |         325.312 |         330.464 |
             335.904 |         341.168 |         346.376 |         351.576 |          356.76 |         361.976 |         367.168 |         372.384 |
               378.8 |         384.264 |         389.448 |         394.688 |         400.072 |         405.872 |           411.2 |           416.4 |
             421.776 |         427.552 |         432.912 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
    ------------------------------------------------------------------------------------------------------------------------------------------------


    gap of hw rx time, us: packets 128:
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          46.872 |           5.696 |           7.344 |           1.008 |     1.84467e+16 |     1.25856e+09 |           0.912 |
               1.136 |            6.56 |     1.84467e+16 |     1.25856e+09 |           5.328 |           5.184 |             5.4 |           6.144 |
         1.84467e+16 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |     1.25856e+09 |           5.184 |           5.232 |           5.296 |
               6.608 |           5.512 |            5.36 |           5.264 |           5.184 |           5.224 |           5.296 |           5.152 |
                5.44 |           5.264 |           5.208 |             5.2 |           5.184 |           5.216 |           5.192 |           5.216 |
               6.416 |           5.464 |           5.184 |            5.24 |           5.384 |             5.8 |           5.328 |             5.2 |
               5.376 |           5.776 |            5.36 |     1.84467e+16 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |

    prio1.txt 
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58


    hw rx time, us: packets 128:
    relative abs time 1914411547728 ns
    first packet abs time 1914411547728 ns
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          10.544 |          17.352 |          52.408 |     1.84467e+16 |          69.336 |          70.264 |     1.84467e+16 |
              85.768 |           86.68 |          87.616 |          94.456 |          95.584 |          97.072 |         105.208 |     1.84467e+16 |
             117.752 |         123.544 |         128.872 |         134.152 |          139.64 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
             161.952 |         167.248 |     1.84467e+16 |     1.84467e+16 |         183.232 |         188.576 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |          322.36 |         327.608 |          339.12 |
             344.768 |         350.008 |         355.312 |           360.6 |          366.08 |         371.288 |          376.72 |         381.944 |
             387.224 |         392.432 |         397.712 |         402.992 |         408.616 |         413.952 |         419.176 |          424.48 |
             429.656 |          434.84 |         440.024 |           445.2 |          450.52 |         455.616 |         461.976 |         467.304 |
             472.528 |         477.776 |         482.976 |         488.152 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
         1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |     1.84467e+16 |
    ------------------------------------------------------------------------------------------------------------------------------------------------


    gap of hw rx time, us: packets 128:
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          10.544 |           6.808 |          35.056 |     1.84467e+16 |     1.91441e+09 |           0.928 |     1.84467e+16 |
         1.91441e+09 |           0.912 |           0.936 |            6.84 |           1.128 |           1.488 |           8.136 |     1.84467e+16 |
         1.91441e+09 |           5.792 |           5.328 |            5.28 |           5.488 |     1.84467e+16 |               0 |               0 |
         1.91441e+09 |           5.296 |     1.84467e+16 |               0 |     1.91441e+09 |           5.344 |     1.84467e+16 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |     1.91441e+09 |           5.248 |          11.512 |
               5.648 |            5.24 |           5.304 |           5.288 |            5.48 |           5.208 |           5.432 |           5.224 |
                5.28 |           5.208 |            5.28 |            5.28 |           5.624 |           5.336 |           5.224 |           5.304 |
               5.176 |           5.184 |           5.184 |           5.176 |            5.32 |           5.096 |            6.36 |           5.328 |
               5.224 |           5.248 |             5.2 |           5.176 |     1.84467e+16 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
                   0 |               0 |               0 |               0 |               0 |               0 |               0 |               0 |
    ------------------------------------------------------------------------------------------------------------------------------------------------
    max val(#4) = 18446742159297952.00us
    min val(#22) = 0.00us
    peak-to-peak = 18446742159297952.00us
    mean +- RMS = 1016749658279961.88 +- 4209743133591792.00 us

    frame size: 80
    number of packets: 128
    RAW RATE = 0.00kbps, PPS = 0.0

    NOTE: here due to plget version time difference is printed in wrong format (eg. 1.84467e+16 ).

  • As above mentioned observation  forgot to add setup i used 

    Case 1 - Am62 to Am62 (without switch)

    Case 2- Am62 -switch -Am62 (without any vlan configuration)

    Case 3- Am62 - switch -Am62 (Vlan configuration only in switch )

    Case 4- Am62 -switch -Am62  (Vlan configuration in all boards )

  • It seems that in Case 4, when VLAN configuration in all boards, there is packets received in the second Am62 board.

    Can you try configuring the TAS with all the gates open?
    I'm assuming that the packets transmitted by the first Am62 board is not getting queued properly causing the TAS to prevent them from going out the switch.
    If we configure the TAS enabled and all the gates open, then packets should be received by the second Am62 board.

    Do you have a Wireshark capture of the packets transmitted by the Am62 board? I'm not familiar with the packets the Am62 boards are generating.

  • Hai ,

    you asked  "Do you have a Wireshark capture of the packets transmitted by the Am62 board? I'm not familiar with the packets the Am62 boards are generating. for this "

    i am just using PLGET  utility for generate and measure time delay in traffic please refer the below link for any doubts about plget usage in am62 

    https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/11_01_05_03/exports/docs/linux/Foundational_Components/Kernel/Kernel_Drivers/Network/CPSW-EST.html#am625-sk-acting-as-a-switch-and-implementing-est-schedule 

    ASAP ill update about  the test case

  • Can you configure the schedule traffic, similar to the picture below?
    This is to verify if packets will be received by the second Am62 board, even if scheduled traffic is enabled for that port. Try to flush the dynamic table before generating the packets.

    If you can connect one of the ports of the Am62 board to a network interface in your PC to capture the packet generated in Wireshark this would also help in understanding the issue.


  • Hai karl,

    In this setup (two AM62 boards and one ADIN switch), with VLAN 100 configured on all boards and Time-Sensitive Networking (TSN) / TAS enabled, 
    we observed that data transmission occurred at random cycle times and did not adhere to the configured Global Control List (GCL) timings."

    However, data transaction was still happening because TAS was enabled on the egress port, resulting in a constant average time difference of 12 for all transactions. 
    The failure to achieve the precise GCL timing is due to the GCL gates not being enabled.


    The priority data received in plget with timings:
     === V ===
    Default address can be specified: 01:1B:19:00:00:00 or 01:80:C2:00:00:0E
    SIOCGHWTSTAMP: tx_type was 0; rx_filter was 12
    SIOCSHWTSTAMP: tx_type 0 requested, got 0; rx_filter 10 requested, got 12
    setting ts_flags: 0x58
    new ts_flags: 0x58


    hw rx time, us: packets 128:
    relative abs time 2057419324603 ns
    first packet abs time 2057419324603 ns
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          15.568 |          27.792 |          62.512 |          74.736 |           86.96 |          99.184 |         111.408 |
             123.632 |         135.864 |         148.088 |         160.312 |         172.536 |          184.76 |         196.984 |         209.208 |
             221.432 |         233.656 |          245.88 |         258.104 |          270.32 |         282.544 |         294.768 |             307 |
             319.224 |         331.448 |         343.672 |         355.896 |          368.12 |         380.344 |         392.568 |         404.792 |
             417.016 |          429.24 |         441.464 |         453.688 |         465.912 |         478.136 |          490.36 |         502.584 |
             514.808 |         527.032 |         539.256 |          551.48 |         563.704 |         575.928 |         588.152 |         600.376 |
               612.6 |         624.824 |         637.048 |         649.272 |         661.496 |          673.72 |         685.944 |         698.168 |
             710.392 |         722.616 |          734.84 |         747.064 |         759.288 |         771.512 |         783.728 |         795.952 |
             808.184 |         820.408 |         832.632 |         844.856 |          857.08 |         869.304 |         881.528 |         893.752 |
             905.976 |           918.2 |         930.424 |         942.648 |         954.872 |         967.096 |          979.32 |         991.544 |
             1003.77 |         1015.99 |         1028.22 |         1040.44 |         1052.66 |         1064.89 |         1077.11 |         1089.34 |
             1101.56 |         1113.78 |         1126.01 |         1138.23 |         1150.46 |         1162.68 |          1174.9 |         1187.13 |
             1199.35 |         1211.58 |          1223.8 |         1236.02 |         1248.25 |         1260.47 |          1272.7 |         1284.91 |
             1297.14 |         1309.36 |         1321.58 |         1333.81 |         1346.03 |         1358.26 |         1370.48 |          1382.7 |
             1394.93 |         1407.15 |         1419.38 |          1431.6 |         1443.82 |         1456.05 |         1468.27 |          1480.5 |
             1492.72 |         1504.94 |         1517.17 |          1529.4 |         1541.62 |         1553.85 |         1566.07 |          1578.3 |
    ------------------------------------------------------------------------------------------------------------------------------------------------


    gap of hw rx time, us: packets 128:
    ------------------------------------------------------------------------------------------------------------------------------------------------
                   0 |          15.568 |          12.224 |           34.72 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.232 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.216 |          12.224 |          12.224 |          12.232 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.216 |          12.224 |
              12.232 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.216 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |          12.224 |
              12.224 |          12.224 |          12.224 |          12.232 |          12.224 |          12.224 |          12.224 |          12.224 |
    ------------------------------------------------------------------------------------------------------------------------------------------------
    max val(#3) = 34.72us
    min val(#20) = 12.22us
    peak-to-peak = 22.50us
    mean +- RMS = 12.43 +- 2.01 us

    === V ===

    NOTE : Same time difference observed in all other priority traffic.

    Tcpdumplog capture while transferring:

    0:34:13.641061 ARP, Request who-has 10.5.0.2 tell 169.254.87.66, length 46
    00:34:14.013157 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 0, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013158 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 1, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013158 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 2, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013261 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 3, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013261 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 4, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013261 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 5, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013261 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 6, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013261 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 7, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013261 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 8, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013261 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 9, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013261 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 10, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013337 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 11, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013337 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 12, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013337 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 13, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013337 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 14, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013337 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 15, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013338 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 16, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013338 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 17, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013411 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 18, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013411 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 19, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013412 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 20, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013412 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 21, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013412 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 22, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013412 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 23, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013472 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 24, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013472 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 25, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.013472 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 26, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    :
    :
    :
    :
    :
    :
    :
    :
    00:34:14.014588 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 119, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.014625 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 120, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.014625 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 121, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.014625 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 122, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.014661 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 123, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.014661 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 124, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.014661 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 125, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.014692 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 126, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.014692 PTPv2, v1 compat : yes, msg type : sync msg, length : 44, domain : 0, reserved1 : 0, Flags [none], NS correction : 0, sub NS correction : 0, reserved2 : 0, clock identity : 0x8063ffff0009ba, port id : 1, seq id : 127, control : 0 (Sync), log message interval : 0, originTimeStamp : 57622080789206 seconds, 1953211286 nanoseconds
    00:34:14.647180 ARP, Request who-has 10.5.0.2 tell 169.254.87.66, length 46
    00:34:15.103647 STP 802.1s, Rapid STP, CIST Flags [Proposal, Learn, Forward, Agreement], length 102
    00:34:16.871390 ARP, Request who-has 10.5.0.2 tell 169.254.87.66, length 46
    00:34:17.103566 STP 802.1s, Rapid STP, CIST Flags [Proposal, Learn, Forward, Agreement], length 102
    00:34:17.642078 ARP, Request who-has 10.5.0.2 tell 169.254.87.66, length 46
    00:34:18.416686 IP 169.254.87.66.netbios-ns > 169.254.255.255.netbios-ns: UDP, length 50



    Here also same transaction observed for other two traffic also .

    Switch table (Flush dynamic table) with or without is same observation. 

    Am i observing or expecting the wrong outcome .

  • Can you share a system block diagram of you configuration?
    Are you also still using the same configuration?

  • Hai ,

    here the system block diagram of my test setup 

    Configuration part in Both AM62 boards i am configuring Vlan 100

    ADIN Configuration

    step 1 -Vlan 100 added for port 1 and 2 as learn and forward,

    step 2-

     

    step 3-

    these are the configuration i used in above case,

    In early replay i mentioned "The failure to achieve the precise GCL timing is due to the GCL gates not being enabled." but its wrong i enabled queue one all gates, i forgot to mention.

  • Hi Dhevak,

    if the traffic is being received on the board 2, then it could be that they are getting queued to Gate 0.

    You can try comparing the results of gate 0 is open or close, if you would be able to receive frames.

    Is there a way to verify if the frames have a VLAN tag and what priority they have?

    For the time synchronization, PTP packets are normally queued to Gate 7, you need to open gate 7 in your cycle time.

    Regards,

    Karl

Reply
  • Hi Dhevak,

    if the traffic is being received on the board 2, then it could be that they are getting queued to Gate 0.

    You can try comparing the results of gate 0 is open or close, if you would be able to receive frames.

    Is there a way to verify if the frames have a VLAN tag and what priority they have?

    For the time synchronization, PTP packets are normally queued to Gate 7, you need to open gate 7 in your cycle time.

    Regards,

    Karl

Children
  • Hi Dhevak,
    I wanted to follow up on the TSN configuration.
    Were you able to verify the VLAN tags, priorities, and gate states as suggested earlier?
    If the issue is resolved, that's great!
    If not. let me know where things stand.
    Regards,
    Karl

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.