Any update on the above query? could you please provide ADIN driver at u-boot level?
Hi Monika,
The ADIN1300 part has IEEE 802.3 compliant MII, RMII and RGMII MAC interfaces, the registers also comply.
It should work with the generic PHY driver implementation in u-boot.
Are you replacing the KSZ9031RNX with the ADIN1300 in a new design? Would you be able to share the schematic for the customized board that is mentioned?
Best Regards,
Mark
Hello Mark,
Yes we are replacing KSZ9031RNX with the ADIN1300 in a new design. With the changes to "mii control" register in the u-boot, we can get RXC clock in u-boot of 25MHZ. (generic driver)
When complete BSP is booted on the device, able to detect eth node as shown below.
******************************************************************************
root@s32g274ardb2:~# [ 5451.150694] 003: s32cc-dwmac 4033c000.ethernet: Set RX/TX clock to 25M
[ 5451.150739] 003: s32cc-dwmac 4033c000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off
root@s32g274ardb2:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:01:02:03:04:05
inet addr:169.254.227.12 Bcast:169.254.255.255 Mask:255.255.0.0
inet6 addr: fe80::a4ac:f63b:d09e:31a2/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:269288 errors:0 dropped:0 overruns:0 frame:0
TX packets:2482 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:23262186 (22.1 MiB) TX bytes:284584 (277.9 KiB)
Interrupt:63 Base address:0x6000
***************************************************************************
ping test is getting failed using udhcpc command, always default setting to static. If tested in static mode also not able to ping
**********************************************************************************
root@s32g274ardb2:~# udhcpc
udhcpc: started, v1.32.0
udhcpc: sending discover
udhcpc: sending discover
udhcpc: sending discover
************************************************************************************
Clock for RXC and TXC are their when complete BSP is up. Could you please help us to fix the issue on priority?
Regards,
Monika