Article What Ethernet PHYs can I use with the switch?

ADI Ethernet PHY products

The following Ethernet PHYs are supported for use with the switch.
Our evaluation boards demonstrate connectivity to some of these PHYs. 
The PHYs can be connected over RMII or RGMII interface to the switch port. 
For an ADI PHY, the switch can help to manage the configuration of the PHY.
For example, consider a multi-speed PHY, when the PHY establishes a link, the switch port gets enabled prompting the switch to interrogate the PHY over the MDIO bus to check what link speed was established. 
With this information, the switch can ensure to adjust the port speed to match. 

  • ADIN1300 - Low Latency, Low power 10/100/1000M Ethernet PHY
  • ADIN1200 - 10/100M Ethernet PHY
  • ADIN1100 - Robust, Industrial, Low Power 10BASE-T1L PHY
  • ADIN1101 - Robust, Industrial, Low Power 10BASE-T1L PHY

What about using other PHY products with the switch?

Non-ADI PHYs could be interfaced to the switch, but will be treated as unmanaged and the switch will not directly configure/interrogate it. 
The host will need to ensure the PHY is configured correctly for operation and ensure that the switch port speed matches the link speed established. 
The host could interface to it through the switch MDIO bus and SES_ReadPhyReg() and SES_WritePhyReg() API calls. 

This places more overhead to the host. 

What about T1S connectivity? Can the switch support connection to a T1S PHY?

Yes, it would be possible to connect a T1S PHY over the RMII MAC interface.
The switch supports Half Duplex which is required by the T1S PHY. 
ADI does not currently have any T1S Ethernet PHY with MAC interface. 
Therefore this PHY would be treated as an Unmanaged PHY, but the host could interface to it through the switch MDIO bus and SES_ReadPhyReg() and SES_WritePhyReg() API calls. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.