Post Go back to editing

KCC's Quiz AQQ300 about Divisibility by 6

1. Quote of the month: "Friendship is like money - easier made than kept" - Samuel Butler

2. New quiz AQQ300 about a divisibility by 6 puzzle 

Good luck and try to be among the first ones!

Please share your answer to view other submitted answers
Parents
  • N^5-n factors into n(n-1)(n+1)(N^2+1).  The first three terms will always have an even number and a multiple of 3,  So the entire function will have 6 as a factor.

    For extra credit, prove that it is also divisible by 5 (and hence 30). 

Reply
  • N^5-n factors into n(n-1)(n+1)(N^2+1).  The first three terms will always have an even number and a multiple of 3,  So the entire function will have 6 as a factor.

    For extra credit, prove that it is also divisible by 5 (and hence 30). 

Children
  • 1

    That's a great observation! Here is my proof:

    n⁵ - n is divisible by 5, because:

    We have n⁵ - n = n(n - 1)(n + 1)(n² + 1).

    We simply need to consider the general form of n: n = 10k ± a, where a = 0, 1, 2, …, 5 and k = 0, 1, 2, …, and evaluate the different possible cases for a:

    If a = 5 or if a = 0, then n is a multiple of 5, so n⁵ - n is divisible by 5 since its expansion contains the factor n.

    If a = 4, then either n + 1 (if n = 10k + 4) or n - 1 (if n = 10k - 4) is divisible by 5, so n⁵ - n is divisible by 5 since its expansion contains (n - 1). (n+1)

    If a = 3, the units digit of n is 3, so n² + 1 ends in 0 and is therefore a multiple of 10, hence n⁵ - n is divisible by 5 since its expansion contains a factor of 10

    If a = 2, n² must end in 4, and n² + 1 is a multiple of 5 since it ends in 5, which implies that n⁵ - n is divisible by 5

    If a = 1, then either n – 1 (if n = 10k + 1) or n + 1 (if n = 10k – 1) is divisible by 5, so n⁵ – n is divisible by 5 since its expansion contains (n – 1)(n + 1).

  • Nice demonstration!
    It also happens to be Fermat's little theorem.  I can't claim to have realized that myself.  After realizing the structure and answer for the original problem, I asked Claude Code to see if there was a more elegant solution.  Calude pointed out the Fermat's little Theorem aspect. 

  • Indeed, it is areal nice demonstration @MileLh !

  • Wow, thus there is somehow a connection to the Fermat's theorem  ; astonishing!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.