Post Go back to editing

KCC's Quizzes AQQ295 about an audio logarithmic volume controller using linear pot - a proposal from Tim O'Brien

1. Quote of the month: "Think like a proton. Always positive" - Unknown

2. New quiz of the month: AQQ295 about a audio logarithmic volume controller using linear pot circuit

A kind proposal from Tim O’Brien (a frequent participant to our quizzes)

Audio volume is usually controlled by a logarithmic (log) potentiometer (pot) to approximate human hearing response.  However true log pots are increasingly hard to source and relatively expensive.  But there is a simple trick to establish an approximation of a log response using a linear pot and a single fixed resistor that’s good for about two decades - provided that the source and load impedances are appropriate to prevent undesirable attenuation at full volume.

One has to build a digital 90 degrees phase splitter circuit giving an in-phase (LO_I) and a quadrature phase (LO_Q) square LO signals phased out 90° one to each other. Among the following 4 circuits, there is one which is not performing that role.

Question: can you localize it and tell why?

1. With a 10K Ohm linear pot what is the value of the parallel fixed resistor R? to establish 10% attenuation at 50% rotation:
     a. assuming zero source and infinite load impedance?
     b. assuming 100 Ohms source and 10K Ohms load impedance?

2. There is no voltage attenuation for 1 a. at full volume, but what is the voltage attenuation at the load at full volume for 1b?

Good luck and try to be among the first ones!

Please share your answer to view other submitted answers
Parents
  • 1a.

    Use a Thevenin equivalent looking back at the pot

    Vs/2 x R?/(2.5K+R?) = 0.1Vs

    R?/(2.5K+R?) = 0.2

    R? = 625Ω

    1b.

    Assuming Rsource=100 and Rload+Load=10K

    Use a Norton equivalent looking back at the pot

    Vs/5.1K = 0.1Vs/5.1K + 0.1Vs/5K + 0.1Vs/R? + 0.1Vs/10K

    10K/5.1K = 1K/5.1K + 1K/5K + 1K/R? + 0.1

    9/5.1 – 0.2 – 0.1 = 1K/R?

    R? = 682.7Ω

    2.

    (Vs-Vload)/100 = Vload/5K + Vload/682.7 ;The 5K equals Rpot||(Rload+Load)

    Vs = Vload + 100Vload/5K + 100Vload/682.7

    Vs/Vload = 1 + 0.02 + 100/682.7 = 1.166477

    Vload/Vs = 0.85728 or 85.73% (a decrease of 14.27% from 1a at full volume)

     

    The above results were verified by simulation in LTspice

  • Big applause to you as well  ! You have also found the right answers!

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.