Post Go back to editing

KCC's Quizzes AQQ295 about an audio logarithmic volume controller using linear pot - a proposal from Tim O'Brien

1. Quote of the month: "Think like a proton. Always positive" - Unknown

2. New quiz of the month: AQQ295 about a audio logarithmic volume controller using linear pot circuit

A kind proposal from Tim O’Brien (a frequent participant to our quizzes)

Audio volume is usually controlled by a logarithmic (log) potentiometer (pot) to approximate human hearing response.  However true log pots are increasingly hard to source and relatively expensive.  But there is a simple trick to establish an approximation of a log response using a linear pot and a single fixed resistor that’s good for about two decades - provided that the source and load impedances are appropriate to prevent undesirable attenuation at full volume.

One has to build a digital 90 degrees phase splitter circuit giving an in-phase (LO_I) and a quadrature phase (LO_Q) square LO signals phased out 90° one to each other. Among the following 4 circuits, there is one which is not performing that role.

Question: can you localize it and tell why?

1. With a 10K Ohm linear pot what is the value of the parallel fixed resistor R? to establish 10% attenuation at 50% rotation:
     a. assuming zero source and infinite load impedance?
     b. assuming 100 Ohms source and 10K Ohms load impedance?

2. There is no voltage attenuation for 1 a. at full volume, but what is the voltage attenuation at the load at full volume for 1b?

Good luck and try to be among the first ones!

Please share your answer to view other submitted answers
Parents
  • To solve the question, we first need to simplify the circuitry.

    We combine all resistors above the wiper to a single one and do the same for the lower. By doing so, we can formulate the solving equation:

    Transforming this equation leads to:

    As a second generalisation we express the upper and lower effective resistor of the potentiometer:

    Finally we need the parallel of the effective lower resistance and the searched resistor:

     Combining the equations and transforming for the lead to:

    Case 1a:

    With

    we get 

    and the searched resistor is:

    Case 1b:

    With

    we get 

    and the searched resistor is:

    Case 2:

    When the wiper is at the upper end we get:

Reply
  • To solve the question, we first need to simplify the circuitry.

    We combine all resistors above the wiper to a single one and do the same for the lower. By doing so, we can formulate the solving equation:

    Transforming this equation leads to:

    As a second generalisation we express the upper and lower effective resistor of the potentiometer:

    Finally we need the parallel of the effective lower resistance and the searched resistor:

     Combining the equations and transforming for the lead to:

    Case 1a:

    With

    we get 

    and the searched resistor is:

    Case 1b:

    With

    we get 

    and the searched resistor is:

    Case 2:

    When the wiper is at the upper end we get:

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.