Post Go back to editing

KCC's Quizzes AQQ294 about a digital phase splitter design

1. Quote of the month: "I've learned that people will forget what you said, people will forget what you did, but people will never forget how you made them roll their eyes" - Robin Williams

2. New quiz of the month: AQQ294 about a digital phase splitter circuit

One has to build a digital 90 degrees phase splitter circuit giving an in-phase (LO_I) and a quadrature phase (LO_Q) square LO signals phased out 90° one to each other. Among the following 4 circuits, there is one which is not performing that role.

Question: can you localize it and tell why?

Good luck and try to be among the first ones!

Edit Notes

Adjusted image size
[edited by: ambugua at 4:00 PM (GMT -5) on 17 Nov 2025]
Please share your answer to view other submitted answers
Parents Reply Children
  • Hi  , the principle of data-clock race issue is a well-known item by the digital circuit designers. When a bloc of linked memory cells have to be triggered at the same time, some cells can receive the active clock later than others (due to routing delays), The only way to be 100% sure is to ensure a cell can be triggered only when its previous cell has NOT received its clock before.