Post Go back to editing

KCC's Quizzes AQQ292 about weighing using 2-plates scale

1. First, the quote of the week: "Some people create their own storms and then get mad when it rains" - Unknown

                                             

 2. New challenge with AQQ292 about using a two-plates scale.

This is a kind proposal from a frequent participant: Herman Neufeld, Analog & Mixed Signals Specialist):

You are asked to design a two-dish scale that weighs amounts of a substance from 1 to 40 grams in integer amounts.

Hence your task is to determine:

  1. What is the minimum number counterweights you need?
  2. What are the weigh values of these counterweights?

These, in order to weigh this substance,

Good luck and try to be among the first ones!

P.S. Please forward such quizzes to friends and colleagues who want also to "relax" their brains...

Please share your answer to view other submitted answers
Parents
  • In simple binary system we can make any number with combination of 2's powers so it could be 1,2,4,8,16,32 with these combination we can achieve any weight. 
    If we want minimum we can try for 3 as well like 1,3,9,27 or may be 4 also 1,4,16,32 but with 4 we can't make 3 or other so no need to try more
    Then 1,3,9,27 will be the minimum possible numbers to achieve the weight example 26 - (27-1) one with 27 and other with 1 example 40 then will keep all four at one side. 
    Maximum achievable weight with this combination will be 40

  • Excellent  , you get it! Congratulations!

Reply Children
No Data