Post Go back to editing

KCC's Quizzes AQQ290 about a triangle coming from the Hell

So, after a long (and deserved) summer vacation, we can suppose your brain is now fully energized and ready to tackle complex problem! 

OK, I know the 2 famous laws about vacations!

1. Vacations are always too short (even if you had 4 weeks)!

2. They always occur in wrong moments (i.e. you were disturbed by any kind of urgencies).

1. First, the quote of the week: "People often say that motivation doesn't last. Well, neither does bathing - that's why we recommend it daily" - Zig Ziglar

                                                        

                                             Source: encrypted-tbn0.gstatic.com/images

2. New challenge: it's a geometry problem, about a triangle that comes from hell... Be careful, there is a trap...

                       

A right triangle has a hypothenuse of 10 cm and an altitude to the hypothenuse of 6 cm.

Question: What is the area of the triangle ABC?

Good luck! And try to be among the first ones!

Also, don't hesitate to share such quizzes with colleagues or friends!

Please share your answer to view other submitted answers
Parents
  • This right angle triangle can not exist, since the height must always be less than half the hypotenuse.
    This is one conclusion from Thales' theorem (=> the height must be equal or less the radius).
    Put simply, it states that all triangles inscribed in a semicircle are right-angled.

    But anyway: If you forget the requirement "right angle" and assume a general triangle, the area is half the product of base and height:
    A = 0.5 * 6cm * 10cm = 30cm^2

Reply
  • This right angle triangle can not exist, since the height must always be less than half the hypotenuse.
    This is one conclusion from Thales' theorem (=> the height must be equal or less the radius).
    Put simply, it states that all triangles inscribed in a semicircle are right-angled.

    But anyway: If you forget the requirement "right angle" and assume a general triangle, the area is half the product of base and height:
    A = 0.5 * 6cm * 10cm = 30cm^2

Children