Post Go back to editing

KCC's Quizzes AQQ287 about throwing 3 dice

1. Quote of the week:"The first five days after the wekend are always the hardest" - unknown

Source: Happy Weekend - Frohes Wochenende - Notiz mit einer Kaffeetasse - Kostenloses Foto auf ccnull.de / ccby.de

2 Our new challenge AQQ287 about throwing 3 dice

Source: upload.wikimedia.org/.../640px-160327_White_dice_09.jpg

The game consists to throw 3 dice and observe the sum S of the 3 top faces. We note P(S) the probability to obtain a sum S.

Questions:

1. For which value of S, the probability P(S) is maximum?

(Example: for 2 dice, S=7 occurs 6 times giving P(7)=0.167 which is the maximum we can get)

 2. Same question as above but in a game with n number of dice.

Good luck and try to be among the first ones!

Also, please forward those quizzes to friends or colleagues who might be interested on such brainstorming!

Please share your answer to view other submitted answers
Parents
  • 1. When you throw 3 dice, max probability is for S=10, 11. You can see this by calculating all the occurrences or by using excel or (better) noting that the average value (expectation value) is 3x (avg outcome 1 dice) = 3x 3.5=10.5 (in the limit of high number of rolls). Since you cannot get a fractional number, max probability will be for the closest integers 10 and 11. The avg outcome of 1 dice is (1+2+3+4+5+6)/6=3.5.

    2. Similarly, for n dice you expect the average outcome= 3.5*n being the most probable outcome.

Reply
  • 1. When you throw 3 dice, max probability is for S=10, 11. You can see this by calculating all the occurrences or by using excel or (better) noting that the average value (expectation value) is 3x (avg outcome 1 dice) = 3x 3.5=10.5 (in the limit of high number of rolls). Since you cannot get a fractional number, max probability will be for the closest integers 10 and 11. The avg outcome of 1 dice is (1+2+3+4+5+6)/6=3.5.

    2. Similarly, for n dice you expect the average outcome= 3.5*n being the most probable outcome.

Children
  • Yes, I agree with your inputs! The relation 3.5*n with n the number of dice can be easily verified for n up to 3. The only pending question is what is the probability (thus the number of times the 3.5 * n result will appear. As I mentioned earlier: I don't have that answer...

  • You have a a discrete probability distribution so you need to calculate the "positive" number of cases and divide it by the total number of cases. For n dice, total number of cases is 6n. Difficult part is to calculate the number of positive cases. Be G(x)= x1 + x2 + x3 +x4 +x5 +xthe polynomial function associated with a single dice. If you have n dice, the total number of ways you can get 3.5*n is the coefficient of x3.5*n  when you, or most probably an algorithm or a tool like wolfram alpha, expand [G(x)](let's assume 3.5*n is an integer, otherwise we follow same process for the closest integers).

    For example, suppose we want to know the probability we get S=35 by rolling 10 dice. By letting wolfram alpha to expand [G(x)]10 , you get 4395256 as a coefficient for x35. So the probability to get S=35 by rolling 10 dice is P(S=35)= 4395256 / 610 0.0727 or something like 7.3%. 

    The max probability will depend on n. I calculated the probability to get S=3.5*n for n=20 and the result is about 5.2%. On the other hand, the probability to get 3.5*n with n=30 is about 4.2%. So the higher the value of n, the lower the max probability, as you might expect by considering that  when n grows, you can get much more different sum results.   

  • Wow, I am impressed  , I was totally ignorant about the wolfram alpha technique. Will dig on it when during my summer vacation... Anywau, many thanks!