Post Go back to editing

KCC's Quizzes AQQ287 about throwing 3 dice

1. Quote of the week:"The first five days after the wekend are always the hardest" - unknown

Source: Happy Weekend - Frohes Wochenende - Notiz mit einer Kaffeetasse - Kostenloses Foto auf ccnull.de / ccby.de

2 Our new challenge AQQ287 about throwing 3 dice

Source: upload.wikimedia.org/.../640px-160327_White_dice_09.jpg

The game consists to throw 3 dice and observe the sum S of the 3 top faces. We note P(S) the probability to obtain a sum S.

Questions:

1. For which value of S, the probability P(S) is maximum?

(Example: for 2 dice, S=7 occurs 6 times giving P(7)=0.167 which is the maximum we can get)

 2. Same question as above but in a game with n number of dice.

Good luck and try to be among the first ones!

Also, please forward those quizzes to friends or colleagues who might be interested on such brainstorming!

Please share your answer to view other submitted answers
Parents
  • 1) Enumeration of the results of each throw gives:
        1 way  for 3
        3 ways for 4
        6 ways for 5
        10 ways for 6
        15 ways for 7
        21 ways for 8
        25 ways for 9
        27 ways for 10
        27 ways for 11
        25 ways for 12
        21 ways for 13
        15 ways for 14
        10 ways for 15
        6 ways for 16
        3 ways for 17
        1 ways for 18
    Two numbers, 10 and 11, have the highest count of 27 so they have the highest chance of occurring. P(S) => 27/216=0.125

    2) For n dice the number(s) with the highest count is(are) at the mid range of S. This gives the most range of selection to equal S.
       Min count = n, Max count = 6n
       Mid range => (6n-n)/2 + n = 3.5n
       S = floor(3.5n) and ceil(3.5n); Both numbers are equal when n is an even integer.
       Example: S=7 for 2 dice and S=10 and 11 for 3 dice.

  • Excellent   and with a solid and clear development, congratulations!

Reply Children
No Data