Post Go back to editing

KCC's Quizzes AQQ287 about throwing 3 dice

1. Quote of the week:"The first five days after the wekend are always the hardest" - unknown

Source: Happy Weekend - Frohes Wochenende - Notiz mit einer Kaffeetasse - Kostenloses Foto auf ccnull.de / ccby.de

2 Our new challenge AQQ287 about throwing 3 dice

Source: upload.wikimedia.org/.../640px-160327_White_dice_09.jpg

The game consists to throw 3 dice and observe the sum S of the 3 top faces. We note P(S) the probability to obtain a sum S.

Questions:

1. For which value of S, the probability P(S) is maximum?

(Example: for 2 dice, S=7 occurs 6 times giving P(7)=0.167 which is the maximum we can get)

 2. Same question as above but in a game with n number of dice.

Good luck and try to be among the first ones!

Also, please forward those quizzes to friends or colleagues who might be interested on such brainstorming!

Please share your answer to view other submitted answers
Parents
  • 1. Mean value of a dice is (1+2+3+4+5+6)/6 = 3.5

    To know the value S where probability P(S) is the maximum, it must be in the mean value.

    Here for 3 dice, mean value is 3.5*3 = 10.5.

    So the value S where probability P(S) is the maximum are 10 and 11 (same probability).

    2. For n number of dice --> S for which P(S) is maximum = 3.5*n.

    It took me a while to figure out the solution, because I initially (and mistakenly) thought the average value of a die was 6 divided by 2. Maybe my background in electronics is to blame... As we always start counting from 0! Wink

    Thanks for this nice puzzle KC !

  • Congratulations  ! The most frequent sum is indeed 3.5 n with n the number of dice. 3.5 n if n is even and 3.5 n +/-0.5 if n is odd. You are in fact nearly there! The only difficult point is what is the probability? I confess I on't have the answer; and count on a miraculous participant...

Reply
  • Congratulations  ! The most frequent sum is indeed 3.5 n with n the number of dice. 3.5 n if n is even and 3.5 n +/-0.5 if n is odd. You are in fact nearly there! The only difficult point is what is the probability? I confess I on't have the answer; and count on a miraculous participant...

Children
No Data