Post Go back to editing

KCC's Quizzes AQQ287 about throwing 3 dice

1. Quote of the week:"The first five days after the wekend are always the hardest" - unknown

Source: Happy Weekend - Frohes Wochenende - Notiz mit einer Kaffeetasse - Kostenloses Foto auf ccnull.de / ccby.de

2 Our new challenge AQQ287 about throwing 3 dice

Source: upload.wikimedia.org/.../640px-160327_White_dice_09.jpg

The game consists to throw 3 dice and observe the sum S of the 3 top faces. We note P(S) the probability to obtain a sum S.

Questions:

1. For which value of S, the probability P(S) is maximum?

(Example: for 2 dice, S=7 occurs 6 times giving P(7)=0.167 which is the maximum we can get)

 2. Same question as above but in a game with n number of dice.

Good luck and try to be among the first ones!

Also, please forward those quizzes to friends or colleagues who might be interested on such brainstorming!

Please share your answer to view other submitted answers
Parents
  • With 3 dice, the range of sums will be from 3 to 18 and the most common sums will be 10 and 11 with equal probability of 27 times out of 216 - P(10) = P(11) = 27/216 = 0.125.

    With n dice, the probability of rolling a particular number on any die is the same and is 1/s where s is the number of sides so 1/6 in this case.  For two dice or more, the number of permutations is given by s^n = 6^2 = 36 for two dice rolls and 6^3 = 216 for three dice rolls.  The sum of the rolls follow a gaussian distribution as there are 6 ways of getting 7 with a 2 rolls but only one way of getting 2 or 12.  The range of values will be integers from n to 6n for a 6-sided dice and the most probable sum will be median value (or two values if the number of dice is odd).

Reply
  • With 3 dice, the range of sums will be from 3 to 18 and the most common sums will be 10 and 11 with equal probability of 27 times out of 216 - P(10) = P(11) = 27/216 = 0.125.

    With n dice, the probability of rolling a particular number on any die is the same and is 1/s where s is the number of sides so 1/6 in this case.  For two dice or more, the number of permutations is given by s^n = 6^2 = 36 for two dice rolls and 6^3 = 216 for three dice rolls.  The sum of the rolls follow a gaussian distribution as there are 6 ways of getting 7 with a 2 rolls but only one way of getting 2 or 12.  The range of values will be integers from n to 6n for a 6-sided dice and the most probable sum will be median value (or two values if the number of dice is odd).

Children