Post Go back to editing

KCC's Quizzes AQQ279 about smart computing

1. Quote of the week: "One advantage of talking to yourself is that you know at least somebody's listening" - Franklin P. Jones

2. New challenge in AQQ279 about a smart computing puzzle:

Knowing that:

X = 13 + 23 + 33 + 43 +… + 113 + 123 = 6084

Question:

What is the value of:

 Y = 23 + 43 + 63… + 223 + 243

Good luck! and try to be among the first ones!

P.S. Don't forget to spread those quizzes around you!

Edit Notes

Remove Image
[edited by: stephenv at 8:36 PM (GMT -5) on 5 Feb 2025]
Please share your answer to view other submitted answers
  • Let's calculate the sum of the cubes of the even numbers from 2 to 24:

    23+43+63+83+103+123+143+163+183+203+223+2432^3 + 4^3 + 6^3 + 8^3 + 10^3 + 12^3 + 14^3 + 16^3 + 18^3 + 20^3 + 22^3 + 24^3

    Breaking it down:

    • 23=82^3 = 8

    • 43=644^3 = 64

    • 63=2166^3 = 216

    • 83=5128^3 = 512

    • 103=100010^3 = 1000

    • 123=172812^3 = 1728

    • 143=274414^3 = 2744

    • 163=409616^3 = 4096

    • 183=583218^3 = 5832

    • 203=800020^3 = 8000

    • 223=1064822^3 = 10648

    • 243=1382424^3 = 13824

    Now, let's sum them all up:

    8+64+216+512+1000+1728+2744+4096+5832+8000+10648+138248 + 64 + 216 + 512 + 1000 + 1728 + 2744 + 4096 + 5832 + 8000 + 10648 + 13824

    Adding these together, the value is:

    492+1728+4096+5832+8000+10648+13824=49000492 + 1728 + 4096 + 5832 + 8000 + 10648 + 13824 = 49000

    Therefore, the sum of 23+43+63+83+...+223+2432^3 + 4^3 + 6^3 + 8^3 + ... + 22^3 + 24^3 is 49,000.

    Pretty neat, isn't it? Smile

  • erm, something didn't go quite well with copying the answer in here, but the sum should be correct.

  • First, you observe that the number of terms of Y is the same as X. Then, you can see that each term in Y is obtained by the respective term in X multiplied by 23. So Y=8*X= 48672.

  • and iof i ask Co-pilot the same question a second time, it gives me a different answer.  Can't trust anyone these days...

    what is the value of 2^3 + 4^3 + 6^3 + 8^3 ... 22^3 + 24^3

    To find the value of the given series, we need to calculate the cube of each term and then sum them all together. Here are the terms in the series with each term cubed:

    23+43+63+83+103+123+143+163+183+203+223+2432^3 + 4^3 + 6^3 + 8^3 + 10^3 + 12^3 + 14^3 + 16^3 + 18^3 + 20^3 + 22^3 + 24^3

    Now let's calculate each term:

    23=843=6463=21683=512103=1000123=1728143=2744163=4096183=5832203=8000223=10648243=138242^3 = 8 \\ 4^3 = 64 \\ 6^3 = 216 \\ 8^3 = 512 \\ 10^3 = 1000 \\ 12^3 = 1728 \\ 14^3 = 2744 \\ 16^3 = 4096 \\ 18^3 = 5832 \\ 20^3 = 8000 \\ 22^3 = 10648 \\ 24^3 = 13824

    Summing these values together:

    8+64+216+512+1000+1728+2744+4096+5832+8000+10648+13824=493368 + 64 + 216 + 512 + 1000 + 1728 + 2744 + 4096 + 5832 + 8000 + 10648 + 13824 = 49336

    Therefore, the value of the series 23+43+63+83+…+223+2432^3 + 4^3 + 6^3 + 8^3 + \ldots + 22^3 + 24^3 is 49,336

  • This ends up being (2*1)^3 + (2*2)^3 + (2*3)^3 ... = 8*1^3 + 8*2^3 ... = 8(X) = 48,672

  • Stupid Co-pilot: when asked a third time I got *another* wrong answer...   Asking Co-pilot if it was sure, it then confirms 48672 as being correct. Sigh! 

    Thanks NorthBus and thanks gpiarino!!!

  • Adding these values together:

    8+64+216+512+1000+1728+2744+4096+5832+8000+10648+13824=491728 + 64 + 216 + 512 + 1000 + 1728 + 2744 + 4096 + 5832 + 8000 + 10648 + 13824 = 49172

    So, the sum of the cubes of the even numbers from 2 to 24 is 49172.

    Are you sure? Shouldn't the answer be 48,672 ??

    Let me double-check that calculation for you. Let's go through it step by step again.

    2^3 = 8$$ $$4^3 = 64$$ $$6^3 = 216$$ $$8^3 = 512$$ $$10^3 = 1000$$ $$12^3 = 1728$$ $$14^3 = 2744$$ $$16^3 = 4096$$ $$18^3 = 5832$$ $$20^3 = 8000$$ $$22^3 = 10648$$ $$24^3 = 13824

    Adding these values again:

    8+64+216+512+1000+1728+2744+4096+5832+8000+10648+13824=486728 + 64 + 216 + 512 + 1000 + 1728 + 2744 + 4096 + 5832 + 8000 + 10648 + 13824 = 48672

    You're right! The correct sum is 48,672. Thanks for pointing that out!

  • Hi,

    A bit of math:

    2^3+4^3+6^3+\cdots+22^3+24^3=

    (2\cdot1)^3+(2\cdot2)^3+(2\cdot3)^3+\cdots+(2\cdot11)^3+(2\cdot12)^3=

    2^3\cdot1^3+2^3\cdot2^3+2^3\cdot3^3+\cdots+2^3\cdot11^3+2^3\cdot12^3=

    2^3\cdot(1^3+2^3+3^3+\cdots+11^3+12^3)

    X = 13 + 23 + 33 + 43 +… + 113 + 123 = 6084 was given, so

    Y=8\cdot X=8\cdot6084=48672

  • Given:

    X = 13 + 23 + 33 + 43 +… + 113 + 123 = 6084

    Y = 23 + 43 + 63… + 223 + 243

    The equation for Y can be rewritten as...

    Y = (2*1)3 + (2*2) 3 + (2*3) 3 + ... + (2*123)= 6084

    Knowing that (a * b)x = a x b x then...

    Y = 23* 13 + 23 * 23 + ...+ 23 * 123

    Y = 23 (13  + 23 + 33 + … + 123 ), which is 23 (X)

    Y  = 8 * 6084 = 48,672

  • assuming the first sum is true, Im not checking then the sum is 6084X 2^3=48672