Post Go back to editing

KCC's Quizzes AQQ277 about a wrong digital design

* Quote of the week: "Never insult an alligator until after you have crossed the river" - unknown

                                                

* New Quiz AQQ277 about a digital design error:

An unskilled (it's not you) digital designer has to build a circuit that materializes the here above truth table.

He uses the Karnaugh table to generate and simplify the circuit as much as he can.

But obviously he made some mistakes because the circuit does not correspond to the truth table.

Questions:

  1. Can you detect where the error(s) have been introduced?
  2. What is your (correct) solution (it’s possible to get a circuit with only 2 simple gates)

Good luck! And try to be among the first ones (i.e. goodies are associated!)

And, if you know friends or colleagues who deserve to participate in these quizzes as well, tell them!

Please share your answer to view other submitted answers
Parents
  • 1. The errors are introduced by an incorrect use of Karnaugh map: you need to group adjacent cells of "1" (in power of 2 numbers) without "0".

    2. The correct circuit consists of a NAND gate with B as first input and the output of the EX-OR operation between A and C as a second input. 

Reply
  • 1. The errors are introduced by an incorrect use of Karnaugh map: you need to group adjacent cells of "1" (in power of 2 numbers) without "0".

    2. The correct circuit consists of a NAND gate with B as first input and the output of the EX-OR operation between A and C as a second input. 

Children