Post Go back to editing

KCC's quiz AQQ274 about 2 sportsmen running and walking

Two  sportsmen A and B have exactly the same running speed and the same walking speed.

One day they started the same trip to the same place.

Sportsman-A walked for half of the distance and ran for the rest, while

Sportsman-B walked for half the time and ran for the other half of time.

Question: Which sportsman reached the end of the trip first? How do you justify it?

Good luck and try to be among the firsts!

P.S. Pass those quizzes among your colleagues and friends; we all need such small brainstorming time to time!

Please share your answer to view other submitted answers
Parents
  • Take: w the walking speed, r the running speed, d the total distance, t1 the time taken byt the first sportsman and t2, taken by the second sportsman.

    First sportsman:  t1 = (d/2)/w  + (d/2)/r     so  t1=(d/2) ( 1/w +1/r)  = (d/2) (w+r)/(wr)
    Second sportman:  w(t2/2) + r(t2/2) = d    so  t2 =                              2d / (w+r)

    t1/t2  =  1/4  (w+r)^2  / wr.  If that value is 1.0, they both reach the end at the same time.  Less that 1, t1 is less than t2 so the first sportsman arrives first, and if greate than 1, the second sportsman arrives first.



    Clearly, that depends on the ratio of w/r.  If w/r  =1,  the expression leads us to conclude that they both arrive at the same time.
    If we assume running is faster than walking, the expression leads us to conclude that the first sportsman arrives last.

    Have  a = r/w, t1/t2=1/4  (1+a)^2  / a.  When equals to 1, we have   4a = (1+a)^2, leading to a = 1, that is, if running equals walking, both arrive at the same time.
    If we assume running is faster than walking, as with a=2 for example, the expression lead us  9/8, so to conclude that the first sportsman arrives last.  (its time, t1, is larger than t2) 

Reply
  • Take: w the walking speed, r the running speed, d the total distance, t1 the time taken byt the first sportsman and t2, taken by the second sportsman.

    First sportsman:  t1 = (d/2)/w  + (d/2)/r     so  t1=(d/2) ( 1/w +1/r)  = (d/2) (w+r)/(wr)
    Second sportman:  w(t2/2) + r(t2/2) = d    so  t2 =                              2d / (w+r)

    t1/t2  =  1/4  (w+r)^2  / wr.  If that value is 1.0, they both reach the end at the same time.  Less that 1, t1 is less than t2 so the first sportsman arrives first, and if greate than 1, the second sportsman arrives first.



    Clearly, that depends on the ratio of w/r.  If w/r  =1,  the expression leads us to conclude that they both arrive at the same time.
    If we assume running is faster than walking, the expression leads us to conclude that the first sportsman arrives last.

    Have  a = r/w, t1/t2=1/4  (1+a)^2  / a.  When equals to 1, we have   4a = (1+a)^2, leading to a = 1, that is, if running equals walking, both arrive at the same time.
    If we assume running is faster than walking, as with a=2 for example, the expression lead us  9/8, so to conclude that the first sportsman arrives last.  (its time, t1, is larger than t2) 

Children