New challenge is here! It's AQQ259 related to a tunable or adjustable amplifier:

The above circuit is a tunable or adjustable gain amplifier. The opamp used is
considered as ideal (i.e. infinite open loop gain, infinite input resistance and
zero output impedance).
Questions:
1. For given R1, R2 and P, at which wiper position α, Vout = 0 volt?
2. Versus Vin, what is the dynamic range of Vout?
Good luck! And try to be among the first ones!
P.S. Don't hesitate to spread those weekly quizzes to colleagues or friends (we need more participants)!
1. alpha= R2/(R1+R2)
2. Vout can span from Vin to (-R2/R1) * Vin
You use the simple relations for an ideal inverting and not inverting opamp. On the non inverting input, you have the partition between (1-alpha)*P and alpha*P, so you end up in the relation Vout= ((-R2/R1) + (1+R2/R1)*alpha)) * Vin. From this relation you can get the answers.