Post Go back to editing

KCC's Quiz AQQ259 about a tunable gain amplifier

New challenge is here! It's AQQ259 related to a tunable or adjustable amplifier:

The above circuit is a tunable or adjustable gain amplifier. The opamp used is

considered as ideal (i.e. infinite open loop gain, infinite input resistance and

zero output impedance).

Questions:

1. For given R1, R2 and P, at which wiper position α, Vout = 0 volt?

2. Versus Vin, what is the dynamic range of Vout?

Good luck! And try to be among the first ones!

P.S. Don't hesitate to spread those weekly quizzes to colleagues or friends (we need more participants)!

Edit Notes

Edit text
[edited by: emassa at 2:12 PM (GMT -4) on 26 Apr 2024]
Please share your answer to view other submitted answers
Parents Reply Children
  • Bingo  , you get it! Congratulations!

  • I'm a little confused: It seems like this quiz was first released back in April 2024? Has the quiz been running until now (April 2025), or has it been restarted? Maybe I missed it in the first place?!

    Looking through the first few answers, in my opinion @retireEE had a very good answer to the quiz, and there are many other really good answers as well.

    By the way, did anyone mention that there is also a limit to the Vin voltage range? If the opamp is a rail-to-rail input, NI+ and IN- can be operated in the entire range between -Ecc and +Ecc, but not below or above. This puts a limit on the voltage range Vin can have.

    Br Stefan

  • Agree with you  ! In fact there are many other limitations that were negleted: Vin, Ecc, -Ecc, opamp leakage etc. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.