KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
New challenge is here! It's AQQ259 related to a tunable or adjustable amplifier:

The above circuit is a tunable or adjustable gain amplifier. The opamp used is
considered as ideal (i.e. infinite open loop gain, infinite input resistance and
zero output impedance).
Questions:
1. For given R1, R2 and P, at which wiper position α, Vout = 0 volt?
2. Versus Vin, what is the dynamic range of Vout?
Good luck! And try to be among the first ones!
P.S. Don't hesitate to spread those weekly quizzes to colleagues or friends (we need more participants)!
1. Vout is 0V at α = R2/(R1+R2)
2. at α = 0: Vout = -Vin * R2/R1
at α = 1: Vout = Vin * (1-(R2/R1))
...and of course, Vout is limited to +Ecc max. / -Ecc min.
1. Vout is 0V at α = R2/(R1+R2)
2. at α = 0: Vout = -Vin * R2/R1
at α = 1: Vout = Vin * (1-(R2/R1))
...and of course, Vout is limited to +Ecc max. / -Ecc min.
Thanks Roland! Agree with your answer 1. But are you sure about question 2? You probably made a typo in an equation when calculating Vout for alpha=1... May be you can recheck?
Oops, I see: The correct answer for α = 1 is Vout = Vin
... but this is only true as long as R1 / R2 is > 0 ...
And if R1=R2 you have a nice use case: With the potentiometer you can adjust the gain from +1 to -1. In the mid position the gain is 0.
Well recovered ADIApproved