Post Go back to editing

KCC's Quizzes AQQ258 about a partial eclipse Sun-Moon

1. Quote of the week: "People say nothing is impossible; but I do nothing every day!" - Anonymous

                     

2. New quiz: AQQ258 about a partial eclipse Sun-Moon

     

Some of us (in Dallas) had probably the chance to have observed a total eclipse of the Sun last week.

To celebrate that event in our quizzes, we propose the following related challenge: 

The above pictures describe a partial eclipse between the moon (circle B) and the sun (circle R).

At a certain instant, the eclipse is such that points MNO form a quarter area of circle R; meaning arc MN is a quarter circle).

At that moment, point O is the center of R and the segment OM measures 4 cm.

Question:

What is the area of the portion of blue circle B that is situated outside circle R?

Good luck! And try to be among the firsts!

Kuo-Chang

P.S. Don't hesitate to share those weekly quizzes in EZ to colleagues or friends!

Please share your answer to view other submitted answers
Parents
  • Without diving into proving all the geometric theorems, using Thale's Theorem, one can determine that line segment MN goes through the center of circle B, so if we can determine the distance of MN, we know the area of circle B.  

    This is determined to be MN - sqrt(4^2 + 4^2) = sqrt(32) = 5.66

    If the diameter of the circle B is sqrt(32), then the area of B is B(area) = pi * (1/2 * sqrt(32))^2 = pi * 1/4 * 32 = 8π

    The area of the arc MON = 1/4 * (pi * 4^2) = 4π

    All that leaves is the area of the two blue arcs inside circle R (but not inside arc MON).  This can be found by calculating the area of B minus the square created by flipping angle MON onto B (forming a square) and using 1/2 of that.

    Area of blue arcs inside R = 1/2 * (B(area) - area of MON square) = 1.2 * (8pi - 4^2) = 4π - 8

    Therefore the area of the blue circle outside circle R = 

    ANSWER = 8π - 4π - (4π - 8)  = 4π - 4π + 8 = 8 cm²

    Cheers!

    Brian

Reply
  • Without diving into proving all the geometric theorems, using Thale's Theorem, one can determine that line segment MN goes through the center of circle B, so if we can determine the distance of MN, we know the area of circle B.  

    This is determined to be MN - sqrt(4^2 + 4^2) = sqrt(32) = 5.66

    If the diameter of the circle B is sqrt(32), then the area of B is B(area) = pi * (1/2 * sqrt(32))^2 = pi * 1/4 * 32 = 8π

    The area of the arc MON = 1/4 * (pi * 4^2) = 4π

    All that leaves is the area of the two blue arcs inside circle R (but not inside arc MON).  This can be found by calculating the area of B minus the square created by flipping angle MON onto B (forming a square) and using 1/2 of that.

    Area of blue arcs inside R = 1/2 * (B(area) - area of MON square) = 1.2 * (8pi - 4^2) = 4π - 8

    Therefore the area of the blue circle outside circle R = 

    ANSWER = 8π - 4π - (4π - 8)  = 4π - 4π + 8 = 8 cm²

    Cheers!

    Brian

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.