And here is a new challenge! It's easier than the previous one but still...

Please spread those weekly quizzes among your colleagues!
Also, please be informed awards and goodies are being sent to the frequent winners. Please apologize for the long delay since we do that only 2 times per year!
Certificates of the wins are also sent in paper form; the ones desiring a digital copy, please let us know!
Some statistics about the frequent winners by country origins: (we have also statistics by individuals, but they can be provided on demand and only with own data).

Regards
Kuo-Chang
3 values for x. (log can be of any base)
a) log(5)/log(2)
b) log((-5 + i*sqrt(79))/2) / log(2)
c) log ((-5 - i*sqrt(79))/2) / log(2)
8^x + 2^x = 130, can be changed to 2^(3x) + 2^x = 130
Substitute for m = 2^x, rearrange.
m^3 + m - 130 = 0
(m-5)(m^2 + 5m + 26) = 0
3 values of m,
m = 5, m = (-5 + (i*sqrt(79))) / 2, m = (-5 - (i*sqrt(79))) / 2
Substitute it values back to m = 2^x. Apply log of any base.
log(m)/log(2) = x
8x+2x=130
(23)x+2x=130
(2x)3+2x=130
Let a=2x which results in the cubic equation:
a3+a-130=0
By inspection, the real root is a=5. The two other roots are non-real complex conjugate numbers. See Cardano’s formula in Wikipedia for the calculation of the complex roots.
X=log(a)/log(2)=2.321928095
Bravo Roland,
x=2.321928 is well a solution to the equation, but it is not the only one!
May be you can find them?
8^x + 2^x = 130
Assume 2^x = t then the equation will become t^3+t-130 = 0
So possible value of t will be 5 so then equation will be (t - 5) (t^2+5t+26) = 0.
And t^2+5t+26 will give us imaginary roots because discrimant is 5*5-4*1*26 which is negative so possible value of t is 5
Hence value of x is log5/log2 which is 2.3219
Ans 2.3219
8^x + 2^x = 130
Assume 2^x = t then the equation will become t^3+t-130 = 0
So possible value of t will be 5 so then equation will be (t - 5) (t^2+5t+26) = 0.
And t^2+5t+26 will give us imaginary roots because discrimant is 5*5-4*1*26 which is negative so possible value of t is 5
Hence value of x is log5/log2 which is 2.3219
Ans 2.3219
Thnaks Sona22 fr your prompt feedback!
Yes, 2.3219 is indeed a solution to the equation. BUT there are others! The question was saying all the possible solutions for x (not necessarily real numbers!). may be you can retreive them?