Post Go back to editing

KCC's Quizzes AQQ247 about Chiral Molecules

Dear Brainstormers,

This week quiz is on a domain that is totally different with what we, actors in electronics, use to see...

It is related to atoms arrangement in molecules, and more particularly in cases of chirality.

Molecules having the same atoms, connected in the same way, having the same apparent chemical functions can, sometime, be different! Such molecules are called chiral. They can interact differently with light or with other components.

Take the following examples:

The usual trick used is when the image of the chiral molecule cannot be superposed (like our left and right hands): the molecule is chiral.

 Question: on the 7 following products, which ones are chiral and which are not (a-chiral):

 

Good luck!



Hide Replies
[edited by: StephenV at 8:13 PM (GMT -5) on 8 Nov 2023]
Please share your answer to view other submitted answers
Parents
  • It's time to publish the official (and hopefully) the right answers! This quiz is indeed twisting our brains... One needs to have a good 3-D imagination to figure out which molecules are chiral or a-chiral.... 

    May did fnd correctly molecules 3, 4 and 6 being chiral, but molecule is also chiral! This is amazing because molecule 7 is quasi identical to molecule 5 bt this allter is a-chiral!

    Anyhow congratulations to  , and   who approach closely the right answers!

    Now, be prepared for the next challenge!

Reply
  • It's time to publish the official (and hopefully) the right answers! This quiz is indeed twisting our brains... One needs to have a good 3-D imagination to figure out which molecules are chiral or a-chiral.... 

    May did fnd correctly molecules 3, 4 and 6 being chiral, but molecule is also chiral! This is amazing because molecule 7 is quasi identical to molecule 5 bt this allter is a-chiral!

    Anyhow congratulations to  , and   who approach closely the right answers!

    Now, be prepared for the next challenge!

Children
No Data