Post Go back to editing

KCC's Quizzes AQQ247 about Chiral Molecules

Dear Brainstormers,

This week quiz is on a domain that is totally different with what we, actors in electronics, use to see...

It is related to atoms arrangement in molecules, and more particularly in cases of chirality.

Molecules having the same atoms, connected in the same way, having the same apparent chemical functions can, sometime, be different! Such molecules are called chiral. They can interact differently with light or with other components.

Take the following examples:

The usual trick used is when the image of the chiral molecule cannot be superposed (like our left and right hands): the molecule is chiral.

 Question: on the 7 following products, which ones are chiral and which are not (a-chiral):

 

Good luck!



Hide Replies
[edited by: StephenV at 8:13 PM (GMT -5) on 8 Nov 2023]
Please share your answer to view other submitted answers
Parents
  • With  a single carbon atom, the criteria often used is to see it one of the 4 companions of the C atom is duplicated. 
    If the three companions are different, there is a "left" version and a "right" version of the molecule  (like the Cartesian x-y-z axis can be left hand or right hand version).
    So, 1, 3, and 4 have and a left and a right version, while molecule 2 has a single version.

    With two carbon atoms, things are a little bit more complex 
    Molecule 6 is the easiest one (with 2 carbons) since the carbons do have different companions than the other:   
                C of the left:   OH, COH , Cl, and the second carbon GROUP  
                C  of the right: OH,  CH3, CH3  and the first carbon GROUP
    So, for each carbon, each carbon has 4 different companions, and the previous criteria is applicable.

    BUT it 3 companions of the two carbons are mutually the same (as for molecule 5 and 7) that becomes more complex since the "carbon GROUP" companion may or may not carry the decision.

    If we look straight from a companion to one of the C atoms, the 3 other companions can be at 12 o'clock, 4 and 8 while, for the second C atom, its three other companions can be at the same matching position, OR, and often more stable, be at  2 o'clock, 6 and 10. So they will be spatially different. But if we take OFF (don't consider) that possibility, since we can turn the molecule around the single bound between the two C, then:


    molecule 5 has the two carbons in a mirror like but nothing forbids the OH of one C to be in opposition of the COOH  or of the CH3.
    (And indeed, the single bound C-C  is said to be stiffer, in "torsion", than say, a double bound as in ethylene HH C =  C HH  )
    So, here, molecule 5  MAY be chiral... or not, given the possible stiff arrangements (and the "attraction/repulsion" of the companions facing each other, or at 60 degree phase of facing each other)
    Molecule 7 is easier that molecule 5 since while each carbon has the same three other companions, they are NOT in the same order:  if one is  in the order  a-b-c, or b-c-a, or c-a-b (considering the possible rotation along the single bound between the two C atoms), the other has the order a-c-b, or c-b-a, or b-a-c  and so, has definitively a "left" and a "right" version.

    So.  has a POSSIBLE left and right version:   1, 3, 4, 5*, 6 and 7
            are (possibly) not:  2 and 5*

  • Typo in the second sentence, it should be :  if the FOUR companions are different, there is a "left" version and ...

Reply Children
No Data