Post Go back to editing

KCC's quizzes AQQ235 about a bipolar common emitter amplifier - a kind proposal from our colleague Martin Walker

Apologize for our non-technical audience since this quiz is more for our FAEs...

A kind proposal from our colleague Martin Walker, ADI Product Marketing Engineer, UK:

Most of our electronic engineers have seen this sort of circuit in their first year study time using a bipolar transistor in its 3 famous basic configurations: common emitter, common collector and common base.

Here above is a common emitter configuration.

Conditions:

  • Vcc = 6V
  • Vout = 3V
  • Tc = 25°C

Q1 is a BJT NPN with current gain β of several hundreds.

RB1 and RB2 are large compared to RC and RS

 Questions :

  1. Is there enough information to work out the gain of this circuit?
  2. If so, what is the voltage gain of the circuit?
  3. Is it a good amplifier?
  4. If not, what would you do to mitigate for its limitations?

Again, many thanks Martin!

Edit Notes

Hide replies until user replies
[edited by: emassa at 2:19 PM (GMT -4) on 22 May 2023]
Please share your answer to view other submitted answers
Parents
  • 1. Given the conditions, the transistor should be in its linear region. Assuming small signal voltage gain is what we mean by gain "Av= vout / vs", then we need the Rc value to evaluate Av= beta * Rc / hie (hie is the input impedance in the BJT hybrid parameters model)

    2. Av= beta * Rc / hie ( Rs considered negligeable)

    3. Very sensitive to temperature variations

    4. You can add a resistor between emitter and ground (that will introduce a negative feedback for stabilization) and maybe a capacitor in parallel. 

  • Merci Gaetano! Answers 1, 3 and 4 are fully correct! On question 2, may be if you elaborate further you can come to a gain expression that gives Ac independent of beta (if beta is large, above 80; which is the case with standard BJTs like BC107, BC108 or BC109 having beta of several hundreds. But let's see our coming other feedback!

  • Hi Kuo-Chang, you can write down Av= -Rc / re (with re equal to the input resistance looking into the emitter terminal with base grounded) but you still have a strong dependency of the voltage gain from beta. Starting from the definition of re:= delta Vbe / delta Ib, you can prove re= hfe / hie or beta / hie. So variations of beta reflects on re and on Av. Different situation with a resistor Re added between the emitter terminal and ground. In this case, with high values of beta, you have Av= - Rc / Re and and a relative independency from beta thanks to the negative feedback. 

Reply
  • Hi Kuo-Chang, you can write down Av= -Rc / re (with re equal to the input resistance looking into the emitter terminal with base grounded) but you still have a strong dependency of the voltage gain from beta. Starting from the definition of re:= delta Vbe / delta Ib, you can prove re= hfe / hie or beta / hie. So variations of beta reflects on re and on Av. Different situation with a resistor Re added between the emitter terminal and ground. In this case, with high values of beta, you have Av= - Rc / Re and and a relative independency from beta thanks to the negative feedback. 

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.