Post Go back to editing

KCC's Quizzes : AQQ234 - Sum of even integers

The sum S of positive even integers starting from 2 to n (even) is described as :

                           S = 2 + 4 + 6 + 8 +… n where the last element n is even.

 Questions:

  1. What is the general formula (function of n) giving a such sum?
  2. Give the sum with n = 5298


Hide replies until user replies
[edited by: emassa at 1:29 PM (GMT -4) on 5 May 2023]
Please share your answer to view other submitted answers
Parents
  • <NOPE, I BELIEVE THIS IS INCORRECT.  I need to go back and spend more time on this.>

    I'm noticing that the total given any n, call it T(n), is just n(n+1) as per below...

    n 1 2 3 4 5
    2n 2 4 6 8 10
    T(n) 2 6 12 20 30
    n(n+1) 2 6 12 20 30

    So, the formula is T(n) = n * (n+1)

    For n = 5298, T(n) = 5298 * 5299 = 28,074,102

    Not very scientific but I think it's correct.

  • Hi Brian, 

    Thanks for your prompt reply.

    Well, I think you have been a little bit too fast. In effect the trick is you assume here n is the number of terms in the sequence while n is the last even integer in the sequence! For example for n=6, S should be 0+2+4+6 = 12 and not 6(6+1) = 42

Reply
  • Hi Brian, 

    Thanks for your prompt reply.

    Well, I think you have been a little bit too fast. In effect the trick is you assume here n is the number of terms in the sequence while n is the last even integer in the sequence! For example for n=6, S should be 0+2+4+6 = 12 and not 6(6+1) = 42

Children
No Data