Post Go back to editing

KCC's Quizzes : AQQ234 - Sum of even integers

The sum S of positive even integers starting from 2 to n (even) is described as :

                           S = 2 + 4 + 6 + 8 +… n where the last element n is even.

 Questions:

  1. What is the general formula (function of n) giving a such sum?
  2. Give the sum with n = 5298


Hide replies until user replies
[edited by: emassa at 1:29 PM (GMT -4) on 5 May 2023]
Please share your answer to view other submitted answers
Parents
  • n = 1; f(n) = 2 = 1 + 1^2

    n = 2; f(n) = 6 = 2 + 2^2

    n = 3' f(n) = 12 = 3 + 3^2

    n = 4; f(n) = 20 = 4 + 4^2

    ...

    So general formula is f(n) = n + n^2

    Sum with n = 5298 is therefore 28,074,102

  • Oh wait, maybe I haven't quite got this right.  My n is the number in the sequence.  If the n in the question refers to the actual even integer, then I would have to divide this by 2 to get the position in the sequence.  In that case, the answer would be 7,019,850, as 5298 is the 2649th number in the sequence of even integers >0.  In this case I concur with Gaetano.

Reply
  • Oh wait, maybe I haven't quite got this right.  My n is the number in the sequence.  If the n in the question refers to the actual even integer, then I would have to divide this by 2 to get the position in the sequence.  In that case, the answer would be 7,019,850, as 5298 is the 2649th number in the sequence of even integers >0.  In this case I concur with Gaetano.

Children