Post Go back to editing

KCC's Quizzes about Golomb rulers

   

A Golomb ruler is a ruler with a set of marks at integer positions such that no two pairs of marks are at the same distance apart. It has been studied by Salomon W. Golomb, Sidon and Babcock. The theory behind the Golomb set of values are used in radio frequency selection, in radio antenna placement and in current transformers

Each ruler can be characterized by:

  1. The first mark is always 0
  2. Its order : number of marks
  3. Its length : distance between the 2 marks at the extreme sides
  4. The ruler is said perfect when all the distances (integer) can be measured from 0 up to its end
  5. The ruler is said Optimal if no shorter Golomb ruler of the same order exists

The above right picture shows a Golomb ruler of order 4, length 6 and is perfect and optimal. For example, it can measure all the distances from 0 to 6. 1 between marks 0 and 1, 2 between marks 4 and 6, 3 between marks 1 and 4, 4 between marks 0 and 4, etc… up to 6 between marks 0 and 6

Questions:

1. What are the order and the length following Golomb ruler? Is it perfect and optimal?

2. Find at least one Golomb ruler of order 5 and of length below or equal to 13 and that is optimal.

P.S. If you think there are still colleagues or friends (internal or external) you think who can be interested in those quizzes, please let let them know....

Kuo-Chang

  • 1. Order=4, Length=7. This ruler is not perfect (distance=5 is missing) and it is not optimal (e.g. the example ruler has same order but shorter length)

    2. The ruler [0, 1, 4, 9, 11] is of order=5 and length=11 and is optimal. 

  • Hi Kuo-Chang,

    Q1. It is order 4 as it has 4 division markings.  It can measure 1, 2 (3-1), 3, 4 (7-3), 6 (7-1) and 7 but not 5.  So, it is not optimal, because there is a shorter ruler of the same order, the one in the question, and not perfect as it cannot measure 5.

    Q2. I found an optimal ruler with markings at 1, 4, 9 and 11 but it is not perfect as it cannot measure 6:

  • 1.

    Order 4, length 7, not perfect (cannot measure 5) and so, not optimal either. (I assume that to be optimal it must be perfect in the first place.)

    2.


    I got 6 of them of order 6, length 13:  (1, 2, 6, 10), (1, 4, 5, 11), (1, 6, 9, 11), (2, 4, 7, 12), (2, 8, 9, 12)  and (3, 7, 11, 12). 0 and 13 are not mentioned but they are implicit. Sure, if (a, b, c, d) works, then (13-a, 13-b, 13-c, 13-d) works too.

    We canot have an optimal ruler of order 5, length >10 since with the markers:  0, u, v, w, L, we can measure, in addition to the obvious u, v, w, and L :  L-u, L-v, L-w, v-u, w-u and w-v, so, a maximum of 10 possible values, so 10 maximum possible different values.

    There is no solution for L=10, order 5, confirmed by a query in Access. (Take all possible combinations of 3 different numbers from 1 to 9 inclusive, compute the 10 possible expressions given here up, COUNT the DISTINCT results, 9 is the maximum "reacheable" distinct values),

    For L = 9, there are: (1, 2, 6), (1, 4, 7), (2, 5, 8) and (3, 7, 8)

    For L = 8, we have (1, 3, 7), (2, 4, 7), (1, 5, 7), (1, 5, 6), (1, 4, 6), (2, 3, 7), (3, 6, 7) and (1, 2, 5)

    For L = 7, (1, 4, 6), (3, 5, 6), (1, 2,4), .... [ 12 in all  ]

    I may have made an error in my Access queries though, have barely double-check.

  • I fail to see how we get 6.  It is not a marker, 1+6 is not a marker, 4+6 isn't, 9-6 neither 11-6.

  • And ChatGP confirms that there is no perfect Golomb Ruler of length 10, order 5.
    So my Access query was probably right.  :-)

  • Thanks Gaetano for your prompt reply! And I can alreday tell you: bingo! You get it, congratulations!

    For question 2: do you think the ruler is perfect?

  • Hello Michel, I suppose your remark to Gaetano is because 6 is not covered? And that's why that ruler is said optimal but NOT perfect...

  • Congratulation Martin! You get it and are (one more) among the very first ones!

  • Thank you Michel for your detailed development! Concerning your remark about a ruler to be perfect and optimal, I think their definitions don't forbid a ruler to be optimal without being perfect. On question 2, you might have missed the ruler (1,4, 9,11)....

  • Hi Kuo-Chang, the ruler of question 2 is NOT perfect (distance =6 is missing).