Post Go back to editing

KCC's Quizzes AQQ230 about a clock and angle puzzle

In an analog clock, the angle formed by the hour and the minute hands varies constantly.

Questions:

  1. Which angle θ is obtained when it is 5:20 ?
  2. Determine when exactly at around 4, the angle will be exactly 90°?


Hide replies until user replies.
[edited by: emassa at 1:54 PM (GMT -4) on 29 Mar 2023]
Please share your answer to view other submitted answers
Parents
  • For the second question, it is obvious there will be 2 possible solutions: the 90° angle can be made with the minute hand before or after the hour hand! But with the way the question has been asked (i.e. "around 4"), there is one solution better than the other...

Reply
  • For the second question, it is obvious there will be 2 possible solutions: the 90° angle can be made with the minute hand before or after the hour hand! But with the way the question has been asked (i.e. "around 4"), there is one solution better than the other...

Children
No Data