Post Go back to editing

KCC's Quizzes AQQ230 about a clock and angle puzzle

In an analog clock, the angle formed by the hour and the minute hands varies constantly.

Questions:

  1. Which angle θ is obtained when it is 5:20 ?
  2. Determine when exactly at around 4, the angle will be exactly 90°?


Hide replies until user replies.
[edited by: emassa at 1:54 PM (GMT -4) on 29 Mar 2023]
Please share your answer to view other submitted answers
Parents
  • 1. θ = 40°

    Solution:

    θ from 12 for each number = 360° / 12 = 30°

    Hour θ movement for each minute = 30° / 60 = 0.5°

    For 20 minutes,

    number = 4

    θ = 4 (30°) = 120°

    For 5,

    θ = 5 (30°) = 150°

    Hour θ movement = 20 (0.5°) = 10°

    Total = 150° + 10° = 160°

    θ difference = 160° - 120° = 40°

    2. 4:05 (minute is 5.45 to be exact)

    Solution:

    θ from 12 for each number = 360° / 12 = 30°

    Hour θ movement for each minute = 30° / 60 = 0.5°

    θ for each minute = 360° / 60 = 6°

    For 4,

    θ = 4 (30°) = 120°

    Equation for 90°:

    90° = [120° + x (0.5°)] - x (6°)

    90° = [120° + 0.5°x] - 6°x

    6°x - 0.5°x = 120° - 90°

    5.5°x = 30°

    x = 5.45

    Time would be 4:05 (5.45 to be exact)

  • Thanks Mark for your so fast feedback! Rendez-vous next week to compare your answers with the official ones!

Reply Children
No Data