A special coding is used to compress 4-digits numbers into one. Can you crack it by giving the value for the last number (in red)?
8809 = 6 |
5555 = 0 |
7111 = 0 |
8193 = 3 |
2172 = 0 |
8096 = 5 |
6666 = 4 |
1012 = 1 |
1111 = 0 |
7777 = 0 |
3213 = 0 |
9999 = 4 |
7662 = 2 |
7756 = 1 |
9313 = 1 |
6855 = 3 |
0000 = 4 |
9881 = 5 |
2222 = 0 |
5531 = 0 |
3333 = 0 |
2581 = ? |
Each digit in the 4 digit number has a value associated with it, and the result is the sum of those values.
1111, 2222, 3333, 5555, and 7777 all have zero as a result, so 1, 2, 3, 5, and 7 digits are all have a value of zero.
0000, 6666, and 9999 have 4 as a result, so 0, 7 and 9 have a value of 1.
8809 =6, so the digit 8 must have a value of 2 (2+2+1+1)
From the above we now know that 2581=0+0+2+0=2
Each digit in the 4 digit number has a value associated with it, and the result is the sum of those values.
1111, 2222, 3333, 5555, and 7777 all have zero as a result, so 1, 2, 3, 5, and 7 digits are all have a value of zero.
0000, 6666, and 9999 have 4 as a result, so 0, 7 and 9 have a value of 1.
8809 =6, so the digit 8 must have a value of 2 (2+2+1+1)
From the above we now know that 2581=0+0+2+0=2