AI and automation are transforming industries at an unprecedented rate, and engineering is no exception. From optimizing complex systems to enhancing predictive maintenance and accelerating design cycles, intelligent systems are reshaping the future of engineering.
Let’s explore how these advancements might shape the industry:
Which engineering domains do you foresee the most disruptive impact from AI and machine learning in the next decade, and what technologies will drive this change?
How can advanced language models like ChatGPT enhance engineering workflow productivity, particularly in code generation, technical documentation, and complex problem-solving?
Mobile robotics are increasingly integrated with advanced perception systems and real-time decision-making algorithms. How does this influence automation in high-precision manufacturing, logistics optimization, or hazardous environment operations?
We’re eager to hear your expert insights! Share your experiences, technical perspectives, and predictions in the comments below. Let’s explore the future of engineering together!
Tagging members who might be interested in this topic mnaughto alexandergoldstein
I'm currently reading "Thinking Fast and Slow" by Daniel Kahneman. As humans, we have two modes of thought: System 1 which is fast, based on instinct and experience, and often prone to error; and System 2, which is slower, more methodical and based on calculation. As humans, we default to System 1 when we can because it takes less effort, although it is prone to systematic errors and bias. My impression is that LLMs like ChatGPT have the same flaw, they default to their System 1. When I asked ChatGPT about one of KCC's Quiz questions, it came up with an answer that was wrong. When I pointed out the error, it switched its answer. No apology. No mea culpa. Not even a, "your right!" Just like a politician, LLMs seem to prioritize giving an answer, even if it is incorrect, over admitting they don't know or they need more information before they can give an answer. As humans, we're experts in using System 1 and what we really want from AI is for it to do the hard calculation required for System 2. However, currently, it seems AI is as lazy and biased as we are...
MTF_Walker I read and reread this; it’s so true. I tested it myself, and yes, I do want AI to handle the hard work, not the simple or the regurgitation of what I can already do in default thinking mode. Right? I can see the danger in relying on AI 100%, hence the disclaimer that "ChatGPT can make mistakes. Check important info"
MTF_Walker I have had the same experience with ChatGPT when creating a quiz and receiving the wrong answer. I learned not to believe the answer blindly but to research because you are right, there are no apologies..LOL