• December 2025 StudentZone Quiz

    Question 1: How does a current-limiting resistor protect an LED, and how can you calculate the appropriate resistor value using Ohm’s Law? Answer 1: A current-limiting resistor protects an LED…
  • November 2025 StudentZone Quiz Solution

    Question 1: What is the relationship between the gain control elements and distortion? Answer 1: The gain control elements in this circuit are silicon diodes, which are nonlinear. As the gain…
  • October 2025 StudentZone Quiz Solution

    Question 1: These simulations focused on the amplitude of the oscillator’s output. In the ideal case (gain = 3.0), is the output distorted? That is, is it anything other than a perfect sinewave? …
  • April 2025 StudentZone Quiz Solution

    Question 1: What is the main function of a Colpitts oscillator? Answer 1: The main function of a Colpitts oscillator is to generate high frequency sinusoidal signals using an LC circuit with a…
  • September 2025 StudentZone Quiz Solution

    Question 1: What is the main advantage of using a double-balanced mixer (Gilbert Cell) over a single-balanced mixer? Answer 1: A double-balanced mixer provides superior isolation between the LO and…
  • July 2025 StudentZone Quiz Solution

    Question 1: What is a pulsed oscillator? Answer 1: A pulsed oscillator is a circuit that produces periodic pulses of electrical energy, rather than a continuous waveform like a sine or square wave…
  • June 2025 StudentZone Quiz Solution

    Question 1: What is the main function of a Peltz oscillator? Answer 1: The Peltz oscillator is used to generate sinusoidal signals and is especially suited for high frequency applications. Its main…
  • May 2025 StudentZone Quiz Solution

    Question 1: What is the main function of a Clapp oscillator? Answer 1: The Clapp oscillator is designed to generate a stable sinusoidal waveform, typically in the radio frequency (RF) range. It functions…
  • Error in February 2025 Student Zone Hartley Oscillator schematic

    This is not so much a question as it is pointing out a clear error in the Feb 2025 Hartley Oscillator student zone schematics. This is especially a problem for content intended for beginners to learn from…
  • February 2025 StudentZone Quiz Solution

    Question 1: What is the main function of a Hartley oscillator? Answer 1: The Hartley oscillator is used to generate sinusoidal signals at a specific frequency. It is commonly employed in RF…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.