• January 2022 StudentZone Quiz Solution

    Question 1: For the circuit in figure 2, at what voltage does the NMOS devices turn off? Answer 1: By analyzing the plot available in the activity material, we can say that the voltage at which the…
  • March 2022 StudentZone Quiz Solution

    Question: Using Ohm's law and the formula for resistors in parallel, what is the output voltage of the R-2R DAC when inputs D7 and D6 are connected to each combination of ground and 3.3 volts? Please…
  • April 2022 StudentZone Quiz Solution

    Question 1: Can you name an advantage of using optocouplers? Answer 1: A main advantage of using optocouplers in different applications is the complete electrical isolation between input and output…
  • May 2022 StudentZone Quiz Solution

    Question 1: How does the SCR differ from an ordinary rectifier diode? Answer 1: The difference between a SCR and a rectifier diode consists of: The SCR is a 3-terminal device while the diode…
  • June 2022 StudentZone Quiz Solution

    Question 1: Can you name several real-life applications of the active rectifiers? Answer 1: Several real-life applications that use active rectifiers are: switched-mode power supplies photovoltaic…
  • July 2022 StudentZone Quiz Solution

    Question: For circuit in Figure 1, what would be the effect of increasing or decreasing the value of both capacitors? Answer: By increasing the value of both capacitors in Figure 1, the frequency…
  • August 2022 StudentZone Quiz Solution

    Question 1: The output circuitry of a typical TTL logic gate is commonly referred to a totem-pole output because the two output transistors are stacked one above the other like carvings on a totem pole…
  • September 2022 StudentZone Quiz Solution

    Question 1: Can you name and describe other types of logic functions that can be built with CD4007 array? Answer 1: Other types of logic functions that can be built with CD4007 are, for example…
  • October 2022 StudentZone Quiz Solution

    Question 1: For the circuit in Figure 3. fill in the table by setting AWG1 and AWG2 to logic high (+5 V) and low (0 V). Answer 1: The output values for each combination of inputs (A and B) are…
  • November 2022 StudentZone Quiz Solution

    Question 1: Can you name the main usage (application) of a D-type latch? Answer 1: The D-type latch is an electronic device that can store one bit of information, is used mainly in data storage…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.