• October 2019 StudentZone Quiz Solution

    October 2019 StudentZone Quiz Solution Question 1: Using the formula given at step 1, the value of C 1 and the plot presented in Figure 4, compute Scope input capacitance C m . Answer 1: The…
  • September 2019 StudentZone Quiz Solution

    September 2019 StudentZone Quiz Solution Question 1: Considering the Inverting Amplifier in firgure 1.8, compute the gain as a function dependent on R1=1KΩ and R2=4.7KΩ. Answer 1: Consider the…
  • August 2019 StudentZone Quiz Solution

    August 2019 StudentZone Quiz Solution Question: The circuit in Figure 30 produces a positive DC output voltage. How can it be reconfigured to make a negative output voltage? Construct the voltage inverter…
  • July 2019 StudentZone Quiz Solution

    July 2019 StudentZone Quiz Solution Question 1: Taking into consideration the Loop Gain Measurement setup described in Figure 3, which is the purpose of the R2 and R3 in the circuit? Answer 1: …
  • June 2019 StudentZone Quiz Solution

    June 2019 StudentZone Quiz Solution Question 1: Using Ohm's law and the formula for resistors in parallel, what is the output voltage of the R-2R DAC when inputs D7 and D6 are connected to each combination…
  • May 2019 StudentZone Quiz Solution

    May 2019 StudentZone Quiz Solution Question 1: How do you measure and computed the slew rate in the unity-gain buffer configuration? Compare this with the value listed in the OP97 data sheet. Answer…
  • March 2019 StudentZone Quiz Solution

    March 2019 StudentZone Quiz Solution Question 1: Compute the resonant frequency f o for the series RLC using equation (2) and compare it to the measured value. Answer 1: Considering the values…
  • April 2019 StudentZone Quiz Solution

    April 2019 StudentZone Quiz Solution Question: Based on your measured data extract the L C and R for the speaker electrical model shown in figure 1 for the speaker you used. You can measure Rdc with…
  • February 2019 StudentZone Quiz Solution

    February 2019 StudentZone Quiz Solution Question: Compute the cut-off frequency for the RC filters above and compare the values with the measured results and simulation results. Explain any differences…
  • January 2019 StudentZone Quiz Solution

    January 2019 StudentZone Quiz Solution Question 1: Compute the cut-off frequencies for each Band Reject filter constructed using the formula in equations (1) and (2). Compare these theoretical values…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.