December 2018 StudentZone Quiz Solution
Question 1:
Compute the cut-off frequencies for each Band Pass filter constructed using the formula in equations (1) and (2). Compare these theoretical values…
November 2018 StudentZone Quiz Solution
Question 1:
Considering the typical probe schematic presented in Figure 7, determine how the adjustable capacitor value can be computed to compensate the frequency…
October 2018 StudentZone Quiz Solution
Question 1:
Calculate the cut-off frequencies for the RC low pass and RL high pass filter using equations (1) and (2).
Answer 1:
RC filter cut-off frequency…
September StudentZone Quiz Solution
Question 1:
In general, which is the effect of improving the power factor?
Answer:
By improving the power factor, you can maximize current-carrying capacity…
August StudentZone Quiz Solution
Question 1:
Calculate the value of the parasitic capacitance.
Answer 1:
We consider the measured value of period for the self-resonance waveform with a 4.7mH inductor…
June StudentZone Quiz Solution
Please find here the answers for the StudentZone article June 2018.
Question 1:
Using equations (5) and (6) determine the impedance (Z circuit ) and phase ( θ ) relationship…
May StudentZone Quiz Solution
Question 1:
Include plots of I L and V R for different tp values: 2τ ,5τ, 10τ.
Answer:
Before including the plots we need to compute the proper frequency of the input…
April StudentZone Quiz Solution
Question 1:
Calculate the time constant (τ) using equation (1) (R= 2.2KOhm, C=0.01uF) and compare it to the measured values.
Repeat this for other set of R and C values…
March StudentZone Quiz Solution
Question 1:
Using voltage division for the circuit of Figure 2, calculate V L . Compare it to the measured values.
Explain any differences.
Answer 1:
…
February StudentZone Quiz Solution
Question:
Construct the circuit of figure 1. Using the Volt Meter Tool, accurately measure V out for the three input voltages (using the ALM1000 fixed power supply…