December StudentZone Quiz Solution
Question 1:
In figure 5 the maximum power of a solar cell is given. Which physical size does have an influence?
Answer:
Of course, the light intensity has an…
November StudentZone Quiz Solution
Quiz 1:
What is the difference between Full Power Bandwidth and Sample Bandwidth ?
Answer:
Full-power bandwidth is the bandwidth that the converter needs to acquire…
October StudentZone Quiz Solution
Follow the link to the Filter Wizard to answer the questions
http://www.analog.com/designtools/en/filterwizard/
Quiz:
Design a two-stage low-pass Butterworth filter…
September StudentZone Quiz Solution
Question:
Please use a differential input for the AD8422, a gain of 100, a positive supply voltage of 15 V, and a negative supply voltage of –15 V. The reference…
August StudentZone Quiz Solution
Virtual Eval Analog Devices
Question:
What would happen with the AD7124-8, when the programmable gain amplifier is set to 128 and the differential input voltage to…
June StudentZone Quiz Solution
Here are the answers for the June 2017 StudentZone Quiz
Q: Which Noise is generated in a Resistor?
A: White Noise
Thermal noise in an ideal resistor is approximately…
May StudentZone Quiz Solution
Figure 8. Quiz: The three ideal capacitors are charged to the voltages shown. What is the final voltage across the bank after closing S1 and then S2? What is the final…
April StudentZone Quiz Solution
The series combination of the three 12uF capacitors is 12uF/3 = 4uF.
Now you have 4uF in parallel with 4uF on the bottom leg that gives 8uF.
8uF in series with the…
March StudentZone Quiz Solution
What current must the 1.5V source supply to the circuit?
Start from the right and take the Thevenin equivalent of the 3k, 6k resistors, and the 9V source:
Combine…
February StudentZone Quiz Solution
Two experiments are conducted on the same Thevenin equivalent network, and the current, i, is measured for each case. What is the Thevenin equivalent voltage and…