Post Go back to editing

SD Card Set Up

Thread Summary

The user is seeking guidance on setting up and configuring the SD image for the AD-Jupiter_EBZ, including flashing the SD card and setting up the TES SDK on Ubuntu Linux 20.04. The final answer directs the user to create a support case with the Analog Devices Technical Support Team for assistance, as there is no specific support group for this product in EngineerZone.
AI Generated Content
Category: Hardware
Product Number: EBZ

Im just starting out on the AD-Jupiter_EBZ and am confused on how to set up/configure the SD Image.  After creating this account I searched and found so many different variations of Issues.

We bought two of these Jupiters and Im simply trying to configure and IMAGE and /Flash the SD Card.  

Can someone please assist? On the SD Card that came with the Jupiter , it contains what I think are the original files for configuring a variety of hardware projects.

Questions:

Are these files to be kept on the SD Card, because If I flash the SD Card these files will be deleted?

I am running Ubuntu Linux 20.04, 

What sequential steps do I need to correctly FLASH the card?

After I Flash The Card how do I set up and configure the TES SDK?

We need to be able to integrate GNU Radio....

How do I set up the Server so it correctly administers a Profile?

*****I realize these questions have been asked, however I have read and visited the GitHub HDL Repo, and the process seems a bit confusing





Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.