Post Go back to editing

Datasheet questions

Category: Datasheet/Specs
Product Number: AD5235

Hello ,

Thank you for all the excellent products and support.

I am sorry for my ignorance in  electronics, I am a computer scientist. I am working on a circuit for electric guitars. I have been building prototypes based on the DS1882 digipot. I now realize that it's not adequate for my purpose and would like to try to use the AD5235. I have 2 questions:

1. Is the AD5235 compatible with 3.3v digital logic.(SPI)?

2. Can the AD5235 accept +/-7v as analog supplies?   

I realize that this information may be available in the datasheet, but I haven't been able to understand it well enough to find it.   

Thank you for your help and understanding.  

  • Hello, 

    1. Is the AD5235 compatible with 3.3v digital logic.(SPI)?

    The allowed input levels depend on the used supply voltage. The datasheet specifies up to Vdd=5V, and there the thresholds are 2,4V for high level and 0,8V for low level. If you drive the inputs by some 3,3V CMOS output, you should be able to reach these levels. 

    The digital output is a so called open drain output. I.e. you can define the output level by yourself, by wiring the required pullup resistor to the according supply. So if you wire the pullup to the 3,3V net, it should work (at least for not too high SPI frequencies). 

    2. Can the AD5235 accept +/-7v as analog supplies?   

    No, unfortunatelly it can't. That's far beyond its absolute maximum ratings, more than 7V between Vdd and Vss may destroy the chip ...

    best regards

    Achim 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.