Post Go back to editing

FMCOMMS5 on VC707

Hello,

I'd like to launch FMCOMMS5 board on VC707 board, but found that there is no RTL project. So I've generated VC707_fmcomms2 project and lookes and BD.

May I just fix BD tcl sript but adding strings like

ad_connect  axi_ad9361_0/adc_valid_q1   adc_wfifo/din_valid_3

ad_connect  axi_ad9361_0/adc_data_q1    adc_wfifo/din_data_3

ad_connect  axi_ad9361_1/adc_enable_i0  adc_wfifo/din_enable_4

ad_connect  axi_ad9361_1/adc_valid_i0   adc_wfifo/din_valid_4

ad_connect  axi_ad9361_1/adc_data_i0    adc_wfifo/din_data_4

ad_connect  axi_ad9361_1/adc_enable_q0  adc_wfifo/din_enable_5

 

to extend

- Add second  AD9361 core

- Extend ADC and DAC buses to 128

- Extend utilpack data buses

- fix UCF. Here is the main problem. May there is somewhere constraints list, because now I can see only one way - write it manualy, which seems to be not Ok.

Is it all?

Parents
  • That's kind of a bad approach. You should not change the block design.

    Take a look at the fmcomms2 for example, and compare the zc706 and vc707 directory. You will see that the difference is just the base block design, the system_top file and the IO constraints.

    What I would recommend is to use the fmcomms2 projects as reference and try to do the same structure for the  fmcomms5.

    If you have other question feel free to ask.

    Thanks,

    Istvan

Reply
  • That's kind of a bad approach. You should not change the block design.

    Take a look at the fmcomms2 for example, and compare the zc706 and vc707 directory. You will see that the difference is just the base block design, the system_top file and the IO constraints.

    What I would recommend is to use the fmcomms2 projects as reference and try to do the same structure for the  fmcomms5.

    If you have other question feel free to ask.

    Thanks,

    Istvan

Children
No Data