Post Go back to editing

AD9361/FMCOMMS2 on Artix UltraScale+ custom board: RX captures all-zero, ad9361_dig_tune fails at every delay

Thread Summary

The user is experiencing issues with no data transitions on RX data lines when interfacing an Artix U+ FPGA with an FMCOMMS2 AD9361 over FMC. Despite correct SPI communication, PLL locks, and RSSI readings, the RX data path fails to capture any data. The final answer suggests the thread can be closed due to inactivity, but the accompanying answers indicate that the IDDR primitives are instantiated correctly and the VADJ level is 1.8V. The user is advised to check if the RX data path is optimized out and consider family-specific differences in settings.
AI Generated Content
Category: Hardware

Hello,

I'm having issues getting anything visible on the RX data lines coming into the Artix U+ FPGA that interfaces to the FMCOMMS2 AD9361 over FMC. I've got a softcore CPU running the no-os firmware, and SPI to the AD9361 works great, RX DATA_CLK is present and correct (l_clk is legit 61.44MHz).

The dig_tune() is completely broken on ever pair.

Here's what works:

  • SPI: chip_id (0x037)=0x0A, all register R/W clean.
  • All PLLs locked: bbpll_lock=1, rx_vco_lock=1, tx_vco_lock=1.
  • ad9361_init() completes ("AD936x Rev 2 successfully initialized"); all calibrations pass (RX/TX BB filter, TIA, ADC, BB-DC, RF-DC, Tx quad).
  • ENSM in FDD-active (REG_STATE lower nibble = 0xA), RX1_EN=1.
  • RF/analog RX works: rx1_rssi shows real energy (symbol ≈ 10900, preamble ≈ 11150), rx1_rf_gain = 71 dB.
  • RX DATA_CLK is live: recovered byte clock l_clk measures 61.44 MHz (the correct 1R1T LVDS DDR rate) via the core's clock monitor; adc_valid pulses continuously.
  • IDELAY infrastructure reports healthy: refclk 300 MHz, fine tap ≈ 104 ps, ≈ 4.9 sw-taps/UI.
  • Parallel-port config reads correct for LVDS DDR 1R1T: 0x010=0xC0, 0x011=0x00, 0x012=0x10.

Here's what I tried already:

  1. Bad board/card — tried my FMCOMMS2 on a ZCU102 with the stock design and it worked.
  2. Pin mapping  rx_clk/rx_frame/rx_data[5:0] LVDS assignments checked against both the carrier and FMCOMMS2 schematics; all are LVDS DIFF_TERM_ADV TERM_100.
  3. Held in reset — ADC/DAC rstn=0x3 (released); IDDR capture primitives have reset tied off.
  4. ENABLE/TXNRX / ENSM trigger — tried SPI ENSM=FDD and pin-control mode (ENABLE_ENSM_PIN_CTRL + level mode + ENABLE asserted). Both reach FDD-active (0xA); both give 0.
  5. IDELAY calibration / sample phase — full dig_tune incl. the FPGA IDELAY sweep across taps 0–31 on all lanes; no passing window anywhere. Also tried ADC_INIT_DELAY=11 (per zcu102). No change.
  6. IDELAY refclk — 300 MHz (the COUNT-mode value); core reports healthy tap resolution.
  7. 1R1T vs 2R2T mode mismatch — ruled out: l_clk=61.44 MHz is the expected 1R1T rate, RX1_EN=1, core runs R1 (runtime adc_r1_mode). A framing mismatch would yield scrambled non-zero data, not static zero.
  8. Simulation — ADI's fmcomms2 testbench (and my datapath sim) validate the capture logic with idealized timing (TX→RX loopback / injected ADC data) and pass; neither exercises real-silicon LVDS RX capture timing.

Here's a summary of the hdl and no-os Git repos I'm using:

ADI analogdevicesinc/hdl main @ 32e1f9c8 ("library/axi_ad485x: Fix simulation issue")

ADI analogdevicesinc/no-OS main @ 313b6a68 ("drivers: axi_core: axi_dmac: …")

So the ultimate questions:

  1. If the RX DATA_CLK is present and correct but there's no transitions on rx_data and rx_frame, what's going on?
  2. Are there known LVDS RX capture issues with the Artux Ultrascale+ that are different from the ZCU102 Zynq Ultrascale+ that I use as a model to build things for my board?

Please help Slight smile

-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

This is my log I have when my board starts up:

[ad9361_no-os] NEORV32 + AD9361 driver starting...
[ad9361_no-os] Calling ad9361_init()...
ad9361_reset: by GPIO
... [BBPLL + clock chain + all calibrations completed OK] ...
ad9361_set_trx_clock_chain: 983040000 245760000 122880000 61440000 30720000 30720000
ad9361_rx_adc_setup : BBBW 8606895 : ADCfreq 245760000
ad9361_run_calibration: CAL Mask 0x80   # RX BB filter   -> OK
ad9361_run_calibration: CAL Mask 0x40   # TX BB filter   -> OK
ad9361_run_calibration: CAL Mask 0x1    # BB DC offset   -> OK
ad9361_run_calibration: CAL Mask 0x2    # RF DC offset   -> OK
ad9361_run_calibration: CAL Mask 0x10   # TX quad        -> OK
LO leakage: 1  Quadrature Calibration: 1 : rx_phase 26
ad9361_set_tx_atten : attenuation 0 mdB tx1=1 tx2=0
rx_adc: Successfully initialized (40960693 Hz)
ad9361_init : AD936x Rev 2 successfully initialized
[ad9361_no-os] ENSM -> FDD

--- RX capture probe (every stimulus reads exactly 0x0000) ---
PHASE 1  real RX (BIST off):           ADC_STATUS=0x05 link_ok=1; adc_valid 200/200 (100%); ch0_I/Q min=0 max=0
PHASE 2  BIST PRBS_INJ_RX (0x3F4=0x09): link_ok=1; adc_valid 200/200 (100%); ch0_I/Q min=0 max=0
PHASE 3  BIST + CHAN_CNTRL_3 pn_sel=9:  ch0_I/Q min=0 max=0
Chip TX-BB->RX-BB loopback (ad9361_bist_loopback(1), DAC PN9): ch0_I/Q min=0 max=0

--- ad9361_dig_tune(BE_MOREVERBOSE|DO_IDELAY), skipmode=1 (RX) ---
SAMPL CLK: 30720000 tuning: RX
  0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
0:# # # # # # # # # # # # # # # #
1:# # # # # # # # # # # # # # # #
ad9361_dig_tune_delay: Tuning RX FAILED!
RX Lane 0, window cnt 0, start 0, IODELAY set to 0   # rx_data[0]
RX Lane 1, window cnt 0, start 0, IODELAY set to 0   # rx_data[1]
RX Lane 2, window cnt 0, start 0, IODELAY set to 0   # rx_data[2]
RX Lane 3, window cnt 0, start 0, IODELAY set to 0   # rx_data[3]
RX Lane 4, window cnt 0, start 0, IODELAY set to 0   # rx_data[4]
RX Lane 5, window cnt 0, start 0, IODELAY set to 0   # rx_data[5]
RX Lane 6, window cnt 0, start 0, IODELAY set to 0   # rx_frame

--- RX-path diagnostic dump ---
[adc_status]
  l_clk_hz=61441040  (expect 61440000 for 1R1T LVDS DDR)
  idelay refclk_hz=300000000 fine_tap=104ps sw_step=1664ps ui=8137ps sw_taps_per_ui=4.89
  rstn=0x3 status=0x5 link_ok=1  pn_oos=1 pn_err=0
  ch0_I ctrl=0x051 status=0x02 data=0x0000  pn_oos=1 pn_err=0 hdr=0
  ch0_Q ctrl=0x051 status=0x02 data=0x0000  pn_oos=1 pn_err=0 hdr=0
[chip_status]
  parallel_port_conf  0x010=0xC0  0x011=0x00  0x012=0x10   (LVDS, DDR, 1R1T, level frame, IQ swap)
  state (0x017)=0x1A  -> ENSM=FDD (0xA)
  RX1_EN=1 RX2_EN=0   TX1_EN=1 TX2_EN=0
  chip_id (0x037)=0x0A   bbpll (0x05E)=0x81 lock=1
  rx_cp_vco (0x247)=0x02 rx_vco_lock=1   tx_cp_vco (0x287)=0x02 tx_vco_lock=1
  rx1_rf_gain=71 dB   rx1_rssi: symbol=10925 preamble=11150
  rx_sampling_freq=30720000 Hz   tx_sampling_freq=30720000 Hz

Thread Notes

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.