| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 0 hours |
SJagini andrei_g srimoyi MStokowski |
Awaiting Customer Response |
AD9361
Recommended for New Designs
The AD9361 is a high performance, highly integrated radio
frequency (RF) Agile Transceiverâ„¢ designed for use in 3G and
4G base station applications....
Datasheet
AD9361 on Analog.com
Hello,
I'm having issues getting anything visible on the RX data lines coming into the Artix U+ FPGA that interfaces to the FMCOMMS2 AD9361 over FMC. I've got a softcore CPU running the no-os firmware, and SPI to the AD9361 works great, RX DATA_CLK is present and correct (l_clk is legit 61.44MHz).
The dig_tune() is completely broken on ever pair.
Here's what works:
chip_id (0x037)=0x0A, all register R/W clean.bbpll_lock=1, rx_vco_lock=1, tx_vco_lock=1.ad9361_init() completes ("AD936x Rev 2 successfully initialized"); all calibrations pass (RX/TX BB filter, TIA, ADC, BB-DC, RF-DC, Tx quad).REG_STATE lower nibble = 0xA), RX1_EN=1.rx1_rssi shows real energy (symbol ≈ 10900, preamble ≈ 11150), rx1_rf_gain = 71 dB.l_clk measures 61.44 MHz (the correct 1R1T LVDS DDR rate) via the core's clock monitor; adc_valid pulses continuously.0x010=0xC0, 0x011=0x00, 0x012=0x10.Here's what I tried already:
rx_clk/rx_frame/rx_data[5:0] LVDS assignments checked against both the carrier and FMCOMMS2 schematics; all are LVDS DIFF_TERM_ADV TERM_100.rstn=0x3 (released); IDDR capture primitives have reset tied off.ENABLE_ENSM_PIN_CTRL + level mode + ENABLE asserted). Both reach FDD-active (0xA); both give 0.dig_tune incl. the FPGA IDELAY sweep across taps 0–31 on all lanes; no passing window anywhere. Also tried ADC_INIT_DELAY=11 (per zcu102). No change.l_clk=61.44 MHz is the expected 1R1T rate, RX1_EN=1, core runs R1 (runtime adc_r1_mode). A framing mismatch would yield scrambled non-zero data, not static zero.Here's a summary of the hdl and no-os Git repos I'm using:
ADI analogdevicesinc/hdl main @ 32e1f9c8 ("library/axi_ad485x: Fix simulation issue")
ADI analogdevicesinc/no-OS main @ 313b6a68 ("drivers: axi_core: axi_dmac: …")
So the ultimate questions:
Please help
-----------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
This is my log I have when my board starts up:
[ad9361_no-os] NEORV32 + AD9361 driver starting...
[ad9361_no-os] Calling ad9361_init()...
ad9361_reset: by GPIO
... [BBPLL + clock chain + all calibrations completed OK] ...
ad9361_set_trx_clock_chain: 983040000 245760000 122880000 61440000 30720000 30720000
ad9361_rx_adc_setup : BBBW 8606895 : ADCfreq 245760000
ad9361_run_calibration: CAL Mask 0x80 # RX BB filter -> OK
ad9361_run_calibration: CAL Mask 0x40 # TX BB filter -> OK
ad9361_run_calibration: CAL Mask 0x1 # BB DC offset -> OK
ad9361_run_calibration: CAL Mask 0x2 # RF DC offset -> OK
ad9361_run_calibration: CAL Mask 0x10 # TX quad -> OK
LO leakage: 1 Quadrature Calibration: 1 : rx_phase 26
ad9361_set_tx_atten : attenuation 0 mdB tx1=1 tx2=0
rx_adc: Successfully initialized (40960693 Hz)
ad9361_init : AD936x Rev 2 successfully initialized
[ad9361_no-os] ENSM -> FDD
--- RX capture probe (every stimulus reads exactly 0x0000) ---
PHASE 1 real RX (BIST off): ADC_STATUS=0x05 link_ok=1; adc_valid 200/200 (100%); ch0_I/Q min=0 max=0
PHASE 2 BIST PRBS_INJ_RX (0x3F4=0x09): link_ok=1; adc_valid 200/200 (100%); ch0_I/Q min=0 max=0
PHASE 3 BIST + CHAN_CNTRL_3 pn_sel=9: ch0_I/Q min=0 max=0
Chip TX-BB->RX-BB loopback (ad9361_bist_loopback(1), DAC PN9): ch0_I/Q min=0 max=0
--- ad9361_dig_tune(BE_MOREVERBOSE|DO_IDELAY), skipmode=1 (RX) ---
SAMPL CLK: 30720000 tuning: RX
0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f:
0:# # # # # # # # # # # # # # # #
1:# # # # # # # # # # # # # # # #
ad9361_dig_tune_delay: Tuning RX FAILED!
RX Lane 0, window cnt 0, start 0, IODELAY set to 0 # rx_data[0]
RX Lane 1, window cnt 0, start 0, IODELAY set to 0 # rx_data[1]
RX Lane 2, window cnt 0, start 0, IODELAY set to 0 # rx_data[2]
RX Lane 3, window cnt 0, start 0, IODELAY set to 0 # rx_data[3]
RX Lane 4, window cnt 0, start 0, IODELAY set to 0 # rx_data[4]
RX Lane 5, window cnt 0, start 0, IODELAY set to 0 # rx_data[5]
RX Lane 6, window cnt 0, start 0, IODELAY set to 0 # rx_frame
--- RX-path diagnostic dump ---
[adc_status]
l_clk_hz=61441040 (expect 61440000 for 1R1T LVDS DDR)
idelay refclk_hz=300000000 fine_tap=104ps sw_step=1664ps ui=8137ps sw_taps_per_ui=4.89
rstn=0x3 status=0x5 link_ok=1 pn_oos=1 pn_err=0
ch0_I ctrl=0x051 status=0x02 data=0x0000 pn_oos=1 pn_err=0 hdr=0
ch0_Q ctrl=0x051 status=0x02 data=0x0000 pn_oos=1 pn_err=0 hdr=0
[chip_status]
parallel_port_conf 0x010=0xC0 0x011=0x00 0x012=0x10 (LVDS, DDR, 1R1T, level frame, IQ swap)
state (0x017)=0x1A -> ENSM=FDD (0xA)
RX1_EN=1 RX2_EN=0 TX1_EN=1 TX2_EN=0
chip_id (0x037)=0x0A bbpll (0x05E)=0x81 lock=1
rx_cp_vco (0x247)=0x02 rx_vco_lock=1 tx_cp_vco (0x287)=0x02 tx_vco_lock=1
rx1_rf_gain=71 dB rx1_rssi: symbol=10925 preamble=11150
rx_sampling_freq=30720000 Hz tx_sampling_freq=30720000 Hz
CodeWarrior - Moved from FPGA Reference Designs to Support AD9361/AD9363/AD9364. Post date updated from Sunday, May 31, 2026 5:55 AM UTC to Sunday, May 31, 2026 5:55 AM UTC to reflect the move.
SJagini - Moved from Support AD9361/AD9363/AD9364 to FPGA Reference Designs. Post date updated from Sunday, May 31, 2026 5:55 AM UTC to Tuesday, June 2, 2026 1:33 PM UTC to reflect the move.
Hi,
Hard to say.
Any critical warning from the tools?
I don't have access to a Artix ultrascale. In the implemented design are the IDDR primitives istantiated?
hdl/library/axi_ad9361/xilinx/axi_ad9361_lvds_if.v at main · analogdevicesinc/hdl
hdl/library/xilinx/common/ad_data_in.v at main · analogdevicesinc/hdl
Is the RX data path optimized out?
Might be a family difference that needs some different settings....
Andrei
Yup, IDDR is instantiated. Looks very similar to the ZCU102. Continuing debug...
Yup, IDDR is instantiated. Looks very similar to the ZCU102. Continuing debug...