Post Go back to editing

Inferred bus interface 'S_AXI' of definition 'analog.com:interface:if_xcvr_cm:1.0' (from User Repositories)

Thread Summary

The user encountered an issue where Vivado 2025.1 incorrectly inferred a standard AXI LITE interface as an ADI-specific bus when integrating custom RTL code with the AD9083 EVM design. The solution was to add the `X_INTERFACE_PRIORITY_LIST` attribute to the RTL code, specifying `xilinx.com:interface:aximm:1.0` to prevent this inference. This workaround ensures the AXI LITE interface connects correctly to the AXI smartconnect or interconnect.
AI Generated Content
Category: Software
Product Number: AD9083

I'm building a design using the AD9083. I built the reference design for the EVM and now want to move that to our custom board.

When I add my custom RTL code to the project, I get this message from Vivado 2025.1:

INFO: [IP_Flow 19-5107] Inferred bus interface 'S_AXI' of definition 'analog.com:interface:if_xcvr_cm:1.0' (from User Repositories).     

Apparently it now sees the standard AXI LITE interface from my RTL code as some custom ADI bus. As a result, it won't connect it to the AXI smartconnect or interconnect. How do I prevent this from happening?

The port definition of my RTL looks like this:

        -- Miscellaneous
        adc_active    : out std_logic;
        data_sync_start     : in  std_logic;
        data_enable   : in  std_logic;
        -- ADC input interface
        adc_dat_a     : in  std_logic_vector(c_adc_dwidth - 1 downto 0);
        adc_dat_b     : in  std_logic_vector(c_adc_dwidth - 1 downto 0);
        -- AXI4-Stream output interface
        aclk   : in  std_logic; -- sample clock and streaming clock
        m_axis_tvalid : out std_logic;
        m_axis_tready : in  std_logic;
        m_axis_tdata  : out std_logic_vector(c_axis_dwidth - 1 downto 0);

        -- AXI lite register interface
        S_AXI_ARESETN   : in std_logic;
        S_AXI_AWADDR    : in std_logic_vector(C_S_AXI_ADDR_WIDTH-1 downto 0);
        S_AXI_AWPROT    : in std_logic_vector(2 downto 0);
        S_AXI_AWVALID   : in std_logic;
        S_AXI_AWREADY   : out std_logic;
        S_AXI_WDATA     : in std_logic_vector(C_S_AXI_DATA_WIDTH-1 downto 0);
        S_AXI_WSTRB     : in std_logic_vector((C_S_AXI_DATA_WIDTH/8)-1 downto 0);
        S_AXI_WVALID    : in std_logic;
        S_AXI_WREADY    : out std_logic;
        S_AXI_BRESP     : out std_logic_vector(1 downto 0);
        S_AXI_BVALID    : out std_logic;
        S_AXI_BREADY    : in std_logic;
        S_AXI_ARADDR    : in std_logic_vector(C_S_AXI_ADDR_WIDTH-1 downto 0);
        S_AXI_ARPROT    : in std_logic_vector(2 downto 0);
        S_AXI_ARVALID   : in std_logic;
        S_AXI_ARREADY   : out std_logic;
        S_AXI_RDATA     : out std_logic_vector(C_S_AXI_DATA_WIDTH-1 downto 0);
        S_AXI_RRESP     : out std_logic_vector(1 downto 0);
        S_AXI_RVALID    : out std_logic;
        S_AXI_RREADY    : in std_logic

Parents Reply Children
No Data