Post Go back to editing

Data Offload Engine + util_hbm issues when using 8GB external DRAM

Thread Summary

The user encountered synthesis errors with the util_hbm IP core when migrating a design from ZCU102 to a custom PCB with 8GB of external DRAM. The issue was due to the 32-bit ADDR_OFFSET localparam being insufficient for the 33-bit AXI address width. The final answer confirmed this as a bug and suggested increasing the ADDR_OFFSET width to match AXI_ADDR_WIDTH as a workaround.
AI Generated Content
Category: Hardware

Hello!

The combination of the Data Offload Engine and util_hbm ip cores is supposed to be capable of handling 8GB of external DRAM, but after migrating our design from ZCU102 to a new custom PCB with more RAM Resources (8GB) the synthesis of util_hbm fails with the following errors:

When looking into this i found, that ADDR_OFFSET is a local parameter (in util_hbm.v), which in Verilog means 32-bit integer. Since the address width of the axi interface is 33 for 8GB this seems to be the reason for the synthesis failing. 


localparam ADDR_OFFSET = (MEM_TYPE == 1) ? DDR_BASE_ADDDRESS :
       (HBM_SEGMENT_INDEX+i) * HBM_SEGMENTS_PER_MASTER * 256 * 1024 * 1024 ;

(line 262-263, util_hbm.v)

The 32 bit localparam is accessed later like this:

.req_dest_address(ADDR_OFFSET[AXI_ADDR_WIDTH-1:AXI_BYTES_PER_BEAT_WIDTH]),

after the following changes the synthesis finishes successfully.

localparam [AXI_ADDR_WIDTH-1:0] ADDR_OFFSET = (MEM_TYPE == 1) ? DDR_BASE_ADDDRESS :
       (HBM_SEGMENT_INDEX+i) * HBM_SEGMENTS_PER_MASTER * 256 * 1024 * 1024 ;

so my question is: is this a bug or have we made a mistake in our configuration and it should work without this modification?

Parents Reply Children
No Data