Post Go back to editing

GHTE3 Transceiver Setup using ultrascale wizard

Thread Summary

The user encountered incorrect QPLL line rate values when using the Wizard for GTHE3 Transceiver settings with a line rate of 5.9904 GHz, QPLL0, and an actual ref clock of 149.76 MHz. The support engineer confirmed the correct settings should be QPLL0_FBDIV=80, QPLL0_REFCLK_DIV=1, and TXOUT_DIV=2, and suggested ensuring the files are properly updated or removed after deleting the IP in Vivado 2022.2. The user verified the correct values after following the advice.
AI Generated Content
Category: Hardware

Hello,

Using the Wizard for the GTHE3 Transceiver settings seems to generate wrong values when checking with the manual line rate calculation for QPLL (https://docs.amd.com/v/u/en-US/ug576-ultrascale-gth-transceivers). 

I give this to the Wizard: 

Line rate = 5.9904 

PLL Type = QPLL0

Actual ref clock = 149.76

Encoding = 8b/10b

But, when i check the line rate using eq. 2-3 and 2-4 i get:  QPLL Line Rate = 1235.52

using these values from the generated files:

f_ref=149.76

QPLL_REFCLK_DIV=2

QPLL_FBDIV=66

TXOUT_DIV=4

So, my question is why do i see a difference?

Parents Reply Children